2022-11-20 9:33 PM
*** The source tree is not clean, please run 'make ARCH=arm mrproper'
*** in /home/developer-package/stm32mp1-openstlinux-5.10-dunfell-mp1-21-03-31/sources/arm-ostl-linux-gnueabi/linux-stm32mp-5.10.10-r0/linux-5.10.10
***
make[2]: *** [outputmakefile] Error 1
make[1]: *** [/home/developer-package/stm32mp1-openstlinux-5.10-dunfell-mp1-21-03-31/sources/arm-ostl-linux-gnueabi/linux-stm32mp-5.10.10-r0/linux-5.10.10/include/config/auto.conf.cmd] Error 2
make[1]: Leaving directory `/home/developer-package/stm32mp1-openstlinux-5.10-dunfell-mp1-21-03-31/sources/arm-ostl-linux-gnueabi/linux-stm32mp-5.10.10-r0/build'
make: *** [__sub-make] Error 2
2022-11-22 1:27 AM
Hi @AKuma.46
There can be multiple reasons to reach this point :
*** The source tree is not clean, please run 'make ARCH=arm mrproper'
Did you follow wiki and/or README instructions?
You can either try the recommended mrproper ...or restart from a fresh installation.
Olivier
2022-11-24 10:04 PM
Dear @Community member
Thanks for you valuable suggestion, after mrproper this error was resolved. but again came to new error:
cc1: error: cannot load plugin ./scripts/gcc-plugins/arm_ssp_per_task_plugin.so
./scripts/gcc-plugins/arm_ssp_per_task_plugin.so: undefined symbol: _ZN8opt_pass14set_pass_paramEjb
make[2]: *** [scripts/mod/empty.o] Error 1
make[1]: *** [prepare0] Error 2
make[1]: Leaving directory `/developer-package/stm32mp1-openstlinux-5.10-dunfell-mp1-21-03-31/sources/arm-ostl-linux-gnueabi/linux-stm32mp-5.10.10-r0/build'
make: *** [__sub-make] Error 2
Please let me know what's the root of this issue.
Note:
ggc installed version is "gcc (Ubuntu 8.4.0-3ubuntu2) 8.4.0" and Ubuntu version is 20.04
Thanks & Regards
Aniket Kumar
2022-11-25 12:35 AM
Hi @AKuma.46 ,
>> gc installed version is "gcc (Ubuntu 8.4.0-3ubuntu2) 8.4.0"
this is not good and probably root cause as it highlights you probably omit to source the SDK.
Please refer to :
With a correct environnement setup you might get something like :
$CC --version
arm-ostl-linux-gnueabi-gcc (GCC) 11.3.0
Copyright (C) 2021 Free Software Foundation, Inc.
This is free software; see the source for copying conditions. There is NO
warranty; not even for MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.
Hope it help,
Olivier
2022-11-25 4:15 AM
Dear @Community member
We downloaded YOCTO SDK version 3.0.0 and Developer Package 3.0.0 and found gcc version is 9.3.0, please find the details below.
DEVELOPER PACKAGE DETAILS
aniket.kumar@si-rd22:~/developer-package/stm32mp1-openstlinux-5.10-dunfell-mp1-21-03-31/sources/arm-ostl-linux-gnueabi/linux-stm32mp-5.10.10-r0/linux-5.10.10$ source /developer-package/SDK/environment-setup-cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi
aniket.kumar@si-rd22:~p/developer-package/stm32mp1-openstlinux-5.10-dunfell-mp1-21-03-31/sources/arm-ostl-linux-gnueabi/linux-stm32mp-5.10.10-r0/linux-5.10.10$ set |grep CROSS
CROSS_COMPILE=arm-ostl-linux-gnueabi-
aniket.kumar@si-rd22:~/developer-package/stm32mp1-openstlinux-5.10-dunfell-mp1-21-03-31/sources/arm-ostl-linux-gnueabi/linux-stm32mp-5.10.10-r0/linux-5.10.10$ $CC --version
arm-ostl-linux-gnueabi-gcc (GCC) 9.3.0
Copyright (C) 2019 Free Software Foundation, Inc.
This is free software; see the source for copying conditions. There is NO
warranty; not even for MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.
YOCTO SDK DETAILS
aniket.kumar@si-rd22:~/developer-package/SDK/sysroots/x86_64-ostl_sdk-linux/usr/bin/arm-ostl-li nux-gnueabi$ ./arm-ostl-linux-gnueabi-gcc --version
arm-ostl-linux-gnueabi-gcc (GCC) 9.3.0
Copyright (C) 2019 Free Software Foundation, Inc.
This is free software; see the source for copying conditions. There is NO
warranty; not even for MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.
As both YOCTO SDK and Developer package SDK is of same version still we are facing this issue while building linux kernel build.
aniket.kumar@si-rd22-bld72:~/developer-package/stm32mp1-openstlinux-5.10-dunfell-mp1-21-03-31/sources/arm-ostl-linux-gnueabi/linustm32mp-5.10.10-r0/linux-5.10.10$ make ARCH=arm modules O="$PWD/../build"
make[1]: Entering directory `/developer-package/stm32mp1-openstlinux-5.10-dunfell-mp1-21-03-31/sources/arm-ostlinux-gnueabi/linux-stm32mp-5.10.10-r0/build'
GEN Makefile
CC scripts/mod/empty.o
cc1: error: cannot load plugin ./scripts/gcc-plugins/arm_ssp_per_task_plugin.so
./scripts/gcc-plugins/arm_ssp_per_task_plugin.so: undefined symbol: _ZN8opt_pass14set_pass_paramEjb
make[2]: *** [scripts/mod/empty.o] Error 1
make[1]: *** [prepare0] Error 2
make[1]: Leaving directory `/developer-package/stm32mp1-openstlinux-5.10-dunfell-mp1-21-03-31/sources/arm-ostl-nux-gnueabi/linux-stm32mp-5.10.10-r0/build'
make: *** [__sub-make] Error 2
Thankyou
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.