2022-09-22 10:00 AM
Hi ST Community,
I'm trying to build st-weston-image for my stm32mp157f-dk2 board with yocto and the following configuration:
Release: kirkstone
MACHINE = "stm32mp1"
The layers that I use are the following:
BBLAYERS ?= " \
</absolute/path/to/yocto/directory>/poky/meta \
</absolute/path/to/yocto/directory>/poky/meta-poky \
</absolute/path/to/yocto/directory>/poky/meta-yocto-bsp \
</absolute/path/to/yocto/directory>/meta-openembedded/meta-filesystems \
</absolute/path/to/yocto/directory>/meta-openembedded/meta-gnome \
</absolute/path/to/yocto/directory>/meta-openembedded/meta-initramfs \
</absolute/path/to/yocto/directory>/meta-openembedded/meta-multimedia \
</absolute/path/to/yocto/directory>/meta-openembedded/meta-networking \
</absolute/path/to/yocto/directory>/meta-openembedded/meta-oe \
</absolute/path/to/yocto/directory>/meta-openembedded/meta-perl \
</absolute/path/to/yocto/directory>/meta-openembedded/meta-python \
</absolute/path/to/yocto/directory>/meta-openembedded/meta-webserver \
</absolute/path/to/yocto/directory>/meta-openembedded/meta-xfce \
</absolute/path/to/yocto/directory>/meta-st-stm32mp \
</absolute/path/to/yocto/directory>/meta-st-openstlinux \
</absolute/path/to/yocto/directory>/meta-qt5 \
"
No other configuration has been done.
Then when I run de "bitbake st-image-weston" command to start with building process all is ok, but after parsing recipes appears the following error:
ERROR: No recipes in default available for:
</absolute/path/to/yocto/directory>/meta-st-openstlinux/recipes-connectivity/bluez5/bluez5_5.64.bbappend
</absolute/path/to/yocto/directory>/meta-st-openstlinux/recipes-graphics/wayland/weston_10.0.0.bbappend
</absolute/path/to/yocto/directory>/meta-st-openstlinux/recipes-multimedia/gstreamer/gstreamer1.0-libav_1.20.2.bbappend
</absolute/path/to/yocto/directory>/meta-st-openstlinux/recipes-multimedia/gstreamer/gstreamer1.0-plugins-bad_1.20.2.bbappend
</absolute/path/to/yocto/directory>/meta-st-openstlinux/recipes-multimedia/gstreamer/gstreamer1.0-plugins-base_1.20.2.bbappend
</absolute/path/to/yocto/directory>/meta-st-openstlinux/recipes-multimedia/gstreamer/gstreamer1.0-plugins-good_1.20.2.bbappend
I'm completely confused with this error. Does anyone know what this error means?
Thanks in advance.
Solved! Go to Solution.
2022-09-26 11:45 PM
Hello @FBofi.1 ,
Yes this problem is known from ST side since kirkstone version. Now you have to place your distribution package in a very short path of your local system to avoid this issue.
To not loose your last compilation time, when you will create your new <build_folder> after sourcing your environment in your new path, you can copy the sstate-cache of your last build (that failed with file name too long).
In summary:
Kind regards,
Erwan.
2022-09-23 12:14 AM
Hello @FBofi.1 ,
If you kept the standard configuration delivered with OSTL 4.0, it is strange that this error happens.
Can you check if you can detect the recipes with the following command ?
bitbake-layers show-recipes > out.txt
I advice you to put the output of the command in an out.txt file as it can be quite long.
Kind regards,
Erwan.
2022-09-23 4:09 AM
Hello @Erwan SZYMANSKI , Thanks for the quick response
I ran the command you said but i got a similar error. I'm attaching it below:
ERROR: No recipes in default available for:
</absolute/path/to/yocto/directory>/meta-st-openstlinux/recipes-connectivity/bluez5/bluez5_5.64.bbappend
</absolute/path/to/yocto/directory>/yocto/meta-st-openstlinux/recipes-graphics/wayland/weston_10.0.0.bbappend
</absolute/path/to/yocto/directory>/meta-st-openstlinux/recipes-multimedia/gstreamer/gstreamer1.0-libav_1.20.2.bbappend
</absolute/path/to/yocto/directory>/meta-st-openstlinux/recipes-multimedia/gstreamer/gstreamer1.0-plugins-bad_1.20.2.bbappend
</absolute/path/to/yocto/directory>/meta-st-openstlinux/recipes-multimedia/gstreamer/gstreamer1.0-plugins-base_1.20.2.bbappend
</absolute/path/to/yocto/directory>/meta-st-openstlinux/recipes-multimedia/gstreamer/gstreamer1.0-plugins-good_1.20.2.bbappend
Traceback (most recent call last):
File "</absolute/path/to/yocto/directory>/poky/bitbake/bin/bitbake-layers", line 95, in <module>
ret = main()
File "</absolute/path/to/yocto/directory>/poky/bitbake/bin/bitbake-layers", line 85, in main
tinfoil.parse_recipes()
File "</absolute/path/to/yocto/directory>/poky/bitbake/lib/bb/tinfoil.py", line 448, in parse_recipes
self.run_actions(config_params)
File "</absolute/path/to/yocto/directory>/poky/bitbake/lib/bb/tinfoil.py", line 431, in run_actions
raise TinfoilUIException(ret)
bb.tinfoil.TinfoilUIException: 1
As additional information, the repositories where I obtained the layers are the following
https://github.com/STMicroelectronics/meta-st-openstlinux
https://github.com/STMicroelectronics/meta-st-stm32mp
https://github.com/meta-qt5/meta-qt5
https://github.com/openembedded/meta-openembedded
Any other idea what might be going on?
Thanks, best regards.
2022-09-23 5:12 AM
Hello @FBofi.1 ,
If you get all the different layers independently, It is highly possible that some versions are not good or something like this.
What I advice you is to start from Distribution Package article and get the repo with repo init and repo sync commands. With this method, you will have all the right versions for each layers.
Kind regards,
Erwan.
(PS: you can take v22.07.27 instead of v22.06.15 as it corrects some minor bugs)
2022-09-23 5:18 AM
Moreover, with regarding to your Path, it seems to not have:
<absolute_path>/layers/openembedded-core/meta inside that contains gstreamer recipes. Can you check that you have it somewhere in your <layer> folder and check if the layer is well added to your conf ?
Kind regards,
Erwan.
2022-09-23 6:35 AM
Hello @FBofi.1 (Community Member) ,
On the top of what has been mentioned above, the same issue found + workaround.
Regards,
Olivier
2022-09-26 10:00 PM
Hello @Erwan SZYMANSKI , @OlivierK
I tried to build the st-image-weston following the instructions of "Distribution Package article" instead to get repositories separately
The first error was fixed but now the following raises:
E: Failed to fetch store:/mnt/d1/yocto/STM32MPU-Ecosystem-v4.0.0/Distribution-Package/openstlinux-5.15-yocto-kirkstone-mp1-v22.07.27/build-openstlinuxweston-stm32mp1/tmp-glibc/work/stm32mp1-ostl-linux-gnueabi/st-image-resize-initrd/1.0-r0/oe-rootfs-repo/cortexa7t2hf-neon-vfpv4/./Packages Could not create temporary file for /mnt/d1/yocto/STM32MPU-Ecosystem-v4.0.0/Distribution-Package/openstlinux-5.15-yocto-kirkstone-mp1-v22.07.27/build-openstlinuxweston-stm32mp1/tmp-glibc/work/stm32mp1-ostl-linux-gnueabi/st-image-resize-initrd/1.0-r0/apt/lists/partial/_mnt_d1_yocto_STM32MPU-Ecosystem-v4.0.0_Distribution-Package_openstlinux-5.15-yocto-kirkstone-mp1-v22.07.27_build-openstlinuxweston-stm32mp1_tmp-glibc_work_stm32mp1-ostl-linux-gnueabi_st-image-resize-initrd_1.0-r0_oe-rootfs-repo_cortexa7t2hf-neon-vfpv4_._Packages - mkstemp (36: File name too long)
Seems like the directory path name is too long, but I don't understand it because also i followed the indications related to directory structure of STM32MPU Ecosystem in the following link
https://wiki.st.com/stm32mpu/wiki/Example_of_directory_structure_for_Packages
Any suggestions? Also I attach de entire log file to additional information
Thanks, best regards.
2022-09-26 11:45 PM
Hello @FBofi.1 ,
Yes this problem is known from ST side since kirkstone version. Now you have to place your distribution package in a very short path of your local system to avoid this issue.
To not loose your last compilation time, when you will create your new <build_folder> after sourcing your environment in your new path, you can copy the sstate-cache of your last build (that failed with file name too long).
In summary:
Kind regards,
Erwan.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.