2025-01-15 7:17 AM
Hello,
I have a custom board with the STM32MP257FAK processor. I am having issues booting into u-boot from emmc. I can boot into u-boot fine using dfu-util over usb. But once I program in fsbl, ssbl, and meta data into the emmc and try to boot from it I get a error with the metadata partition. See log below.
Any ideas what could cause this error?
Solved! Go to Solution.
2025-01-16 5:47 AM
Resolved the issue.
There was a difference in the .dts file from for the STM32MP25-EV1 board and my custom board with the pin layout for the sdmmc. The evaluation board had this :
&sdmmc2 {
pinctrl-names = "default";
pinctrl-0 = <&sdmmc2_b4_pins_a &sdmmc2_d47_pins_a>;
non-removable;
no-sd;
no-sdio;
st,neg-edge;
bus-width = <8>;
vmmc-supply = <&vdd_emmc>;
vqmmc-supply = <&vddio2>;
status = "okay";
};
/omit-if-no-ref/
sdmmc2_b4_pins_a: sdmmc2-b4-0 {
pins1 {
pinmux = <STM32_PINMUX('E', 13, AF12)>, /* SDMMC2_D0 */
<STM32_PINMUX('E', 11, AF12)>, /* SDMMC2_D1 */
<STM32_PINMUX('E', 8, AF12)>, /* SDMMC2_D2 */
<STM32_PINMUX('E', 12, AF12)>, /* SDMMC2_D3 */
<STM32_PINMUX('E', 15, AF12)>; /* SDMMC2_CMD */
slew-rate = <1>;
drive-push-pull;
bias-pull-up;
};
pins2 {
pinmux = <STM32_PINMUX('E', 14, AF12)>; /* SDMMC2_CK */
slew-rate = <2>;
drive-push-pull;
bias-pull-up;
};
};
/omit-if-no-ref/
sdmmc2_d47_pins_a: sdmmc2-d47-0 {
pins {
pinmux = <STM32_PINMUX('E', 10, AF12)>, /* SDMMC2_D4 */
<STM32_PINMUX('E', 9, AF12)>, /* SDMMC2_D5 */
<STM32_PINMUX('E', 6, AF12)>, /* SDMMC2_D6 */
<STM32_PINMUX('E', 7, AF12)>; /* SDMMC2_D7 */
slew-rate = <1>;
drive-push-pull;
bias-pull-up;
};
};
and I had this :
&sdmmc1 {
pinctrl-names = "default";
pinctrl-0 = <&sdmmc1_pins_mx>;
status = "okay";
/* USER CODE BEGIN sdmmc1 */
non-removable;
no-sd;
no-sdio;
st,neg-edge;
bus-width = <8>;
vmmc-supply = <&vdd_emmc>;
vqmmc-supply = <&vddio2>;
/* USER CODE END sdmmc1 */
};
sdmmc1_pins_mx: sdmmc1_mx-0 {
pins1 {
pinmux = <STM32_PINMUX('D', 8, AF11)>, /* SDMMC1_D7 */
<STM32_PINMUX('D', 9, AF11)>, /* SDMMC1_D6 */
<STM32_PINMUX('D', 10, AF11)>, /* SDMMC1_D5 */
<STM32_PINMUX('D', 11, AF11)>, /* SDMMC1_D4 */
<STM32_PINMUX('E', 0, AF10)>, /* SDMMC1_D2 */
<STM32_PINMUX('E', 1, AF10)>, /* SDMMC1_D3 */
<STM32_PINMUX('E', 2, AF10)>, /* SDMMC1_CMD */
<STM32_PINMUX('E', 4, AF10)>, /* SDMMC1_D0 */
<STM32_PINMUX('E', 5, AF10)>; /* SDMMC1_D1 */
bias-disable;
drive-push-pull;
slew-rate = <1>;
};
pins2 {
pinmux = <STM32_PINMUX('E', 3, AF10)>; /* SDMMC1_CK */
bias-disable;
drive-push-pull;
slew-rate = <3>;
We had to split the pins into two banks like the EV board does. Once we did that we booted fine from emmc. Not sure why that made it work though.
2025-01-16 5:47 AM
Resolved the issue.
There was a difference in the .dts file from for the STM32MP25-EV1 board and my custom board with the pin layout for the sdmmc. The evaluation board had this :
&sdmmc2 {
pinctrl-names = "default";
pinctrl-0 = <&sdmmc2_b4_pins_a &sdmmc2_d47_pins_a>;
non-removable;
no-sd;
no-sdio;
st,neg-edge;
bus-width = <8>;
vmmc-supply = <&vdd_emmc>;
vqmmc-supply = <&vddio2>;
status = "okay";
};
/omit-if-no-ref/
sdmmc2_b4_pins_a: sdmmc2-b4-0 {
pins1 {
pinmux = <STM32_PINMUX('E', 13, AF12)>, /* SDMMC2_D0 */
<STM32_PINMUX('E', 11, AF12)>, /* SDMMC2_D1 */
<STM32_PINMUX('E', 8, AF12)>, /* SDMMC2_D2 */
<STM32_PINMUX('E', 12, AF12)>, /* SDMMC2_D3 */
<STM32_PINMUX('E', 15, AF12)>; /* SDMMC2_CMD */
slew-rate = <1>;
drive-push-pull;
bias-pull-up;
};
pins2 {
pinmux = <STM32_PINMUX('E', 14, AF12)>; /* SDMMC2_CK */
slew-rate = <2>;
drive-push-pull;
bias-pull-up;
};
};
/omit-if-no-ref/
sdmmc2_d47_pins_a: sdmmc2-d47-0 {
pins {
pinmux = <STM32_PINMUX('E', 10, AF12)>, /* SDMMC2_D4 */
<STM32_PINMUX('E', 9, AF12)>, /* SDMMC2_D5 */
<STM32_PINMUX('E', 6, AF12)>, /* SDMMC2_D6 */
<STM32_PINMUX('E', 7, AF12)>; /* SDMMC2_D7 */
slew-rate = <1>;
drive-push-pull;
bias-pull-up;
};
};
and I had this :
&sdmmc1 {
pinctrl-names = "default";
pinctrl-0 = <&sdmmc1_pins_mx>;
status = "okay";
/* USER CODE BEGIN sdmmc1 */
non-removable;
no-sd;
no-sdio;
st,neg-edge;
bus-width = <8>;
vmmc-supply = <&vdd_emmc>;
vqmmc-supply = <&vddio2>;
/* USER CODE END sdmmc1 */
};
sdmmc1_pins_mx: sdmmc1_mx-0 {
pins1 {
pinmux = <STM32_PINMUX('D', 8, AF11)>, /* SDMMC1_D7 */
<STM32_PINMUX('D', 9, AF11)>, /* SDMMC1_D6 */
<STM32_PINMUX('D', 10, AF11)>, /* SDMMC1_D5 */
<STM32_PINMUX('D', 11, AF11)>, /* SDMMC1_D4 */
<STM32_PINMUX('E', 0, AF10)>, /* SDMMC1_D2 */
<STM32_PINMUX('E', 1, AF10)>, /* SDMMC1_D3 */
<STM32_PINMUX('E', 2, AF10)>, /* SDMMC1_CMD */
<STM32_PINMUX('E', 4, AF10)>, /* SDMMC1_D0 */
<STM32_PINMUX('E', 5, AF10)>; /* SDMMC1_D1 */
bias-disable;
drive-push-pull;
slew-rate = <1>;
};
pins2 {
pinmux = <STM32_PINMUX('E', 3, AF10)>; /* SDMMC1_CK */
bias-disable;
drive-push-pull;
slew-rate = <3>;
We had to split the pins into two banks like the EV board does. Once we did that we booted fine from emmc. Not sure why that made it work though.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.