STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Witch STM32 chip for my project ?

Hi everybody!I working on a simple project but with some sensors and co.I'm newbie with the STM32 and I want to try to port the project from the ATmega2560 to the STM32.But witch chip? I need :> SPI for an TFT screen 2.2" (ILI9340C or ILI9341)> SPI f...

DMost by Associate
  • 2952 Views
  • 2 replies
  • 0 kudos

Resolved! STM32MP FMC SRAM & ARM M4

For an application we are investigating this processor and have two questions,We want to connect an external chip to the FMC bus. It is somespecialized ASIC handling some real-time communication.I don't see the option in the STM32Cube to active the F...

Resolved! Could not set DRM mode for screen DSI1/Could not queue DRM page flip on screen DSI1 (Permission denied) for st-example-image-qt

Hi,I have succesfully built a image st-example-image-qt from the DISTRO openstlinux-eglfs.I have deployed the image on sd card, and played it on STM32MP157C-DK2.System is booting without a problem, and the splashscreen was shown.Then, I tried one of ...

Resolved! DFU not detected

HiI got an STM32MP157C-DK2 during the Embedded World.But Windows7 isn't detecting the DFU ... It detects only the STLink (UART) ....Same issue in a Ubuntu-16 (which is running in VirtualBox on the same Windows 7)Any suggestion?Regards Francesco

Resolved! Yocto_SDK Software Version- 1.0.0 for STM32MP151C. Is it suitable for just raw framebuffer implementation?

I downloaded Yocto_SDK Software Version- 1.0.0 for STM32MP151C. The environment setup file name is - "environment-setup-cortexa7t2hf-neon-vfpv4-openstlinux_weston-linux-gnueabi". Does it mean that this SDK is tailored for Wayland implementation? We i...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.