STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to control a GPIO in userspace

Hi: https://wiki.st.com/stm32mpu/wiki/How_to_control_a_GPIO_in_userspace,compiling the user application according to the wiki example while putting it on the board performs an error,how should I deal with the problem?Failed to issue GET LINEHANDLE...

Wjian.1 by Associate II
  • 1292 Views
  • 1 replies
  • 0 kudos

Resolved! How to flash TF-A , u-boot , root file system to SD card without USB with STM32CubeProgrammer

Following Wiki page shows how to flash TF-A , u-boot , root file system to SD card with STM32CubeProgrammer.​https://wiki.st.com/stm32mpu/wiki/STM32CubeProgrammer#How_to_flash_with_STM32CubeProgrammer​In the above wiki page, I can flash ​TF-A , u-boo...

HMasu.1 by Senior
  • 1845 Views
  • 2 replies
  • 0 kudos

Resolved! Does DK2 include NPU (galcore.ko)?

Recently, I bought STM32MP1 DK2 board. Does DK2 board include NPU (Neural Processing Unit)? Can we use ​the NPU device via galcore.ko (Linux kernel module) to run deep learning network models on the DK2 board? Welcome to any hints and comments.​​BR...

ChipHead by Associate III
  • 4717 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.