STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Is it possible to run the qt5 3d demos with a openstlinux-eglfs build (STM32MP157C-DK2)?

I created an eglfs Yocto build that can run the simple Qt5 demos, but I'm seeing fairly high CPU usage and I'm trying to figure out if the GPU is being used. I pondered that the GPU may not accelerate 2D graphics very well and does better with actual...

JWeis.3 by Associate
  • 2527 Views
  • 2 replies
  • 2 kudos

Exit Low Power Mode M4 via CAN

Hi, i have a question regarding to exit the Low Power Mode on CM4. Is it possible that i can exit the CStop or CStandby Mode via an Rx Messages of the CAN Bus, when the CAN Bus is assigned to the M4. Iam confused because almost every Bus is listed in...

YRink.1 by Associate II
  • 3801 Views
  • 1 replies
  • 0 kudos

USART probe error

Hello,I am using stm32mp157c-dk2 board and working on "How to exchange large data buffers with the coprocessor - example" from the wiki:https://wiki.st.com/stm32mpu/wiki/How_to_exchange_large_data_buffers_with_the_coprocessor_-_exampleI need to do so...

MElha.1 by Associate II
  • 2731 Views
  • 2 replies
  • 0 kudos

Multiple Rpmsg Channels

Hi,i just implemented the OpenAMP_tty_echo example for my device. And i just wanna know if i have the right understanding for it. Iam using two virtualUARTS, does this mean that i have two Endpoints over one RPMSG Channel. Or do i have two RPMSG Chan...

YRink.1 by Associate II
  • 2691 Views
  • 1 replies
  • 0 kudos

CM4 SPI problem

I think I have encountered some difficult problems. I hope the engineer of ST can help me.I configured SPI+DMA to CM4 and then created two rPMSGs. RPMSg0 transmitted the data to CA7 in real time and RPMSg1 transmitted the heartbeat signal.When CA7 re...

0693W000007BNaqQAG.png
Yli.8 by Associate II
  • 1027 Views
  • 0 replies
  • 0 kudos

Need support to send sensor data on AWS

Hello ST Community,I had successfully run the "Hello World" code on my STM32MP1 which is based on python by the following link,https://docs.amazonaws.cn/en_us/greengrass/latest/developerguide/module2.htmlI have one sensor connected with STM32MP1. I h...

NPanc.1 by Associate II
  • 1257 Views
  • 1 replies
  • 1 kudos

Resolved! I want to know the difference of device tree compiling the with the Developer Package and Distribution Package.

I want to know the difference of device tree compiling the with the Developer Package and Distribution Package.​I understand that when I create my own machine, I can create device tree by following 2 method. Method 1) Building device trees with Devel...

HMasu.1 by Senior
  • 1740 Views
  • 1 replies
  • 0 kudos

stm32pm1 power failure

Strange issueused power supply 24v, 5AIf we connect debug 3.5 MM cable on debug port, then only unit boots up and taking to kernel command line prompt else it does not boot upI tried taking out LCD display , USB, battery, still above issue thereits a...

Ara.1 by Senior
  • 1479 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.