STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Stop mode does not work as expected

Hi! I am using an STM32MP153 and am working on implementing the STOP mode functionality for my application. The MCU shall wake up on a falling edge on pin PI8. The pin PG15 has an interrupt attached to it for another functionality. Before going into ...

tinova-1 by Associate II
  • 6787 Views
  • 5 replies
  • 0 kudos

Booting custom STM32MP151fAC1 board

Hi All, I'm trying to boot a custom board using the Starter Package through the STM32CubeProgrammer. I'am flashing the SD Card on the board through the UART interface as USB interface(CN7/USB_OTG) is not provided for the board. During this process I'...

MicrosoftTeams-image.png
prik_29 by Associate
  • 3426 Views
  • 4 replies
  • 1 kudos

Resolved! FDCAN in normal mode is not working

Hi!I am using the stm32mp157C-DK2 board to communicate via FDCAN and my idea is to use it as normal mode to send and receive CAN messages. For this I have created a program in stm32cubeide and I enable FDCAN1 with the following parameters (125Kb/s): ...

TArre.1 by Associate III
  • 6024 Views
  • 7 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.