2025-01-19 10:23 PM
Is there a recommended minimum SMT package size and power rating for resistor R4 (8R2) please?
Solved! Go to Solution.
2025-01-19 11:46 PM
R4 is only connected to GND by Q1 for a very short time, defined by the monoflop U1 with R3/C3, so that the heating of R4 is almost negligible depending on its dimensioning. With the approx. 0.4ms (100k, 5.6nF) from AN5861, a resistor size of 0805 is certainly sufficient.
Hope that helps?
Regards
/Peter
2025-01-19 11:46 PM
R4 is only connected to GND by Q1 for a very short time, defined by the monoflop U1 with R3/C3, so that the heating of R4 is almost negligible depending on its dimensioning. With the approx. 0.4ms (100k, 5.6nF) from AN5861, a resistor size of 0805 is certainly sufficient.
Hope that helps?
Regards
/Peter
2025-01-20 12:22 AM
Hi Peter,
Thanks very much.
Kind regards,
Al
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.