cancel
Showing results for 
Search instead for 
Did you mean: 

After extensive evaluation of the stm32mp157-DK2 board in our labs, we are ready to commit to using this board as-is in a longer term project with interested parties in several branches of science. Will this board be available for a few years out?

STild.1
Associate

In our early evaluation phase, the stm32mp157 chip is ideal for our requirements - with the ability to do hard real-time processing with the M4 core but still have a Linux framework to develop interfaces to upstream processing applications. We feel that the DK2 Discovery board can be deployed in developed systems AS-IS until 'hardened' systems are needed for future military, space, and biomedical customers. The instrument technology we are developing is now being considered for phase-2 evaluation and studies with several interested clients but we need to know if the board will be available for a few years. In future 'hardened' systems, we and others will make our own boards using the stm32mp157 chip and request guidance regarding the long-term support commitment for the chip.

Scott Tilden, PhD

U of Arizona

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Peter BENSCH
ST Employee

Thank you for evaluating our STM32MP1!

This family of microprocessors is part of our product longevity program and will be available for a minimum of 10 years.

Although the evaluation boards are expected to be available for a few years, the longevity program does not apply here. Additionally the STM32MP157C-DK2 and STM32MP157F-DK2 are evaluation boards which are intended for evaluation purposes only, as stated in the Terms of Use:

The Evaluation Board shall not be, in any case, directly or indirectly assembled as a part in any production of Yours as it is

solely developed to serve evaluation and testing purposes and has no direct function and is not a finished product.

We wish you success!

When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.