2023-08-21 3:38 AM
u-boot yocto build fails with this message
test -e arch/arm/dts/stm32mp157c-mydemo-mx.dtb || ( \
| echo >&2; \
| echo >&2 "Device Tree Source (arch/arm/dts/stm32mp157c-mydemo-mx.dtb) is not correctly specified."; \
| echo >&2 "Please define 'CONFIG_DEFAULT_DEVICE_TREE'"; \
| echo >&2 "or build with 'DEVICE_TREE=<device_tree>' argument"; \
arch/arm/dts/stm32mp157c-mydemo-mx.dts exists
arch/arm/dts/stm32mp157c-mydemo-mx-u-boot.dtsi exists
stm32mp157c-mydemo.dtb has been added to the Makefile
Any ideas?
2023-09-01 12:25 AM
Hi @edwardmcl ,
Sorry to come late in this thread.
Are you still stuck ? If yes please provide more information about the way you configure and launch Yocto build + complete logs
Thanks
Olivier
2023-09-01 4:00 AM
Hello,
I am facing the same issue as @edwardmcl - are there any solutions?
I mainly followed instructions in https://wiki.st.com/stm32mpu/wiki/How_to_compile_the_device_tree_with_the_Distribution_Package
but it is not working. When I build my image I get that u-boot-stm32mp fails as above . Below my log
make -f /home/luisa/dev/st/st_distro/stdistro/build-try-test1/tmp-glibc/work-shared/stm32mp151a-bitron-som/uboot-source/scripts/Makefile.build obj=arch/arm/dts dtbs
test -e arch/arm/dts/stm32mp151a-bitron-som-mx.dtb || ( \
echo >&2; \
echo >&2 "Device Tree Source (arch/arm/dts/stm32mp151a-bitron-som-mx.dtb) is not correctly specified."; \
echo >&2 "Please define 'CONFIG_DEFAULT_DEVICE_TREE'"; \
echo >&2 "or build with 'DEVICE_TREE=<device_tree>' argument"; \
echo >&2; \
/bin/false)
files
stm32mp151a-bitron-som-mx.dts
stm32mp151a-bitron-som-mx-u-boot.dtsi
are below my building path <builddir>/tmp-glibc/work-shared/stm32mp151a-bitron-som/uboot-source/arch/arm/dts and are as the one below my mx/bitron_som_20634519_06/CA7/DeviceTree/bitron-som/u-boot directory.
What is not clear to me is
1. are YOCTO recipes sufficient to to generate dtb files or should I do manually something additionally?
2. using OpenSTLinux distribution, should I also follow instructions at https://wiki.st.com/stm32mpu/wiki/How_to_configure_U-Boot_for_your_board ?
Attached my mylayer/conf/machine/stm32mp151a-bitron-som.conf file (just extended to .txt for upload)
Looking forward to your answer.
Thank you.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.