2021-12-17 1:31 PM
I didn't change anything in the device tree just compiled the arm-trusted-firmware-v2.4-stm32mp-r2 instead of arm-trusted-firmware-v2.4-stm32mp-r1 and I get the following on UART:
PANIC at PC : 0x2ffcfd2b
What is different between the two versions?
Solved! Go to Solution.
2024-09-08 4:44 AM - edited 2024-09-08 7:25 AM
Hello Bernard,
We are using Dunfell V3.1.
According to the thread above, the patch directs to drivers/regulator/regulator_core.c in project arm-trusted-firmware-v2.4-stm32mp-r1 (or r2).
However, in our project, we have this path:
./arm-trusted-firmware-2.4/drivers/st/regulator/stm32mp_regulator.c
Is this the right path for the file in the patch?
Please advise.
thanks,
Gil
2024-09-09 2:46 AM
Hello Gil,
the proposed patch is in the core part of the regulator (then not specific to stm32 device) so should be no issue to apply it on your release.
Please see the architecture from wiki V3 documentation: https://wiki.st.com/stm32mpu-ecosystem-v3/wiki/Regulator_overview
2025-05-22 2:04 AM
hello Bernard,
I am replying to you just now, since we are trying now to fix the issue now.
In-case we are not able to apply the patch, there is a solution you originally suggested (before the patch was available):
In our case, our custom board connects v3v3 (BUCK4) to both vmmc and vqmmc supplies.
Should I remove both lines (vmmc-supply = <&v3v3>; vqmmc-supply = <&v3v3>) from the TF-A dts?
thanks,
Gil
2025-05-26 1:40 AM
Hello Gil,
The goal was to avoid a new switch off/on of the sdcard (just after the Rom code one). So only vmmc-supply.
2025-05-26 5:50 AM - edited 2025-06-19 3:23 AM
Hello Bernard,
As I understand, the line vmmc-supply = <&v3v3> connects the supply v3v3 to the alias vmmc-supply, and the TF-A uses this alias to toggle the v3v3 supply. This toggling is not allowing the eMMC to respond correctly to CMD13 (SDMMC init), because it takes time for the supply to become stable after the toggle.
Am I correct here?
We use this line in the eMMC Flash node.
Is the same toggling done also for vqmmc-supply = <&v3v3>?
Shouldn't we also avoid doing that in the TF-A?
thank you
Gil
2025-06-04 8:52 AM - edited 2025-06-19 3:22 AM
Hello Bernard,
I'd highly appreciate if you can answer my message above.
thank you
Gil
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.