2020-03-18 11:21 AM
Hi,
I try use optee with weston image and I find that:
Once the machine is defined with MACHINE_FEATURES += "optee" and the distro is set with DISTRO_FEATURES_append = " optee ", building the OpenSTLinux distribution will provide all necessary binaries to populate and boot with OP-TEE feature.
But after build image with bitbake "bitbake st-image-weston" I don't have Flashlayout_*-optee.tsv in flashlayout_st-image-weston folder.
Do I have add some special macro to generate optee.tsv ?
For now I have only this in conf/local.conf
MACHINE_FEATURES += "optee"
DISTRO_FEATURES_append = " optee "
I add that I have generated:
tee-header_v2-stm32mp157c-dk2-optee.stm32
tee-pageable_v2-stm32mp157c-dk2-optee.stm32
tee-pager_v2-stm32mp157c-dk2-optee.stm32
2020-03-19 3:53 AM
Hi Adrian,
i've just tried and I see file e.g. FlashLayout_sdcard_stm32mp157c-dk2-optee.tsv generated as expected.
Do you use latest 1.2.0?
Could you please verify that you correctly updated both files stm32mp1.conf and openstlinux.inc?
BR,
Milan
2020-03-20 2:21 AM
hi, thanks for answer I solved the problem. That as you written I got the wrong version and in stm32mp1-disco.conf I have commented BOOTSCHEME_LABELS += "optee". now it's works ;)
Thanks !
Adrian
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.