2024-08-29 11:01 PM
Hi Every One
i am facing the issue to find the pins of PWM in the (STM32mp157f-dk2 ), i configured the PWM channel in device tree and pwm channel is visible in /sys/class/pemchip0/pwm , so i need to collect the input from the pins but which pin is connected to PWM i do not know , could you please help me out this.
(this is my my output form the board terminal )
root@stm32mp1:/sys/class/pwm/pwmchip0/pwm0# ls
capture duty_cycle enable period polarity power uevent
root@stm32mp1:/sys/class/pwm/pwmchip0/pwm0#
I Need
1. how to use pin and which pin i need to connect
2. i want to collect the input prom the PWM.
3. and the should be show on the terminal.
if i am wrong and any thing missing , please correct me
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.