2020-10-21 1:12 AM
Hi all,
I am trying to switch to using FIT images and I am looking at the example .its file here:
I am trying to understand why 0xC0008000 is used for the load address/entry point. If I understand correctly:
Wouldn't it be possible to skip the relocation in step 3 by choosing a different address for the load address/entry point in the FIT image?
Thanks,
Guillermo
Solved! Go to Solution.
2020-10-22 2:55 AM
Hi,
when I test FIT, I experiment Image (with or without compression) and zImage.
And when I upstream the patch, I let the value 0xC0008000 required for "Image" (kernel image without embedded decompression).
With zImage it is working but the kernel decompression need to move the kernel code before decompression at final address 0xC0008000.
A good choice to load zImage is 0xC4000000.
It is aligned with "fdt_addr_r=0xc4000000" in stm32mp1.h to allow 32MB kernel image, so it will work with 32MB FIT.
You have 3 solution it is possible to avoid relocation during decompression:
1/ load Zimage at correct location = 0xC4000000
kernel {
description = "Linux kernel";
data = /incbin/("zImage");
type = "kernel";
arch = "arm";
os = "linux";
compression = "none";
load = <0xC4000000>;
entry = <0xC4000000>;
hash-1 {
algo = "sha1";
};
};
2/ use Image.gz , lets U-Boot decompress the kenel = "Image" at the correcct location (it is my preferred solution that avoid the first copy)
kernel {
description = "Linux kernel";
data = /incbin/("Image.gz");
type = "kernel";
arch = "arm";
os = "linux";
compression = "gzip";
load = <0xC0008000>;
entry = <0xC0008000>;
hash-1 {
algo = "sha1";
};
};
3/ use zImage in place (inside the FIP) : with 0xCC offset in my example but this offset depends on FIT content so it is less flexible
kernel {
description = "Linux kernel";
data = /incbin/("zImage");
type = "kernel";
arch = "arm";
os = "linux";
compression = "none";
load = <0xC20000cc>;
entry = <0xC20000cc>;
hash-1 {
algo = "sha1";
};
};
Or you can used uncomprressed kernel: "Image" (time with decompression need to be chacked)
kernel {
description = "Linux kernel";
data = /incbin/("Image");
type = "kernel";
arch = "arm";
os = "linux";
compression = "none";
load = <0xC0008000>;
entry = <0xC0008000>;
hash-1 {
algo = "sha1";
};
};
Regards
Patrick
2020-10-22 2:55 AM
Hi,
when I test FIT, I experiment Image (with or without compression) and zImage.
And when I upstream the patch, I let the value 0xC0008000 required for "Image" (kernel image without embedded decompression).
With zImage it is working but the kernel decompression need to move the kernel code before decompression at final address 0xC0008000.
A good choice to load zImage is 0xC4000000.
It is aligned with "fdt_addr_r=0xc4000000" in stm32mp1.h to allow 32MB kernel image, so it will work with 32MB FIT.
You have 3 solution it is possible to avoid relocation during decompression:
1/ load Zimage at correct location = 0xC4000000
kernel {
description = "Linux kernel";
data = /incbin/("zImage");
type = "kernel";
arch = "arm";
os = "linux";
compression = "none";
load = <0xC4000000>;
entry = <0xC4000000>;
hash-1 {
algo = "sha1";
};
};
2/ use Image.gz , lets U-Boot decompress the kenel = "Image" at the correcct location (it is my preferred solution that avoid the first copy)
kernel {
description = "Linux kernel";
data = /incbin/("Image.gz");
type = "kernel";
arch = "arm";
os = "linux";
compression = "gzip";
load = <0xC0008000>;
entry = <0xC0008000>;
hash-1 {
algo = "sha1";
};
};
3/ use zImage in place (inside the FIP) : with 0xCC offset in my example but this offset depends on FIT content so it is less flexible
kernel {
description = "Linux kernel";
data = /incbin/("zImage");
type = "kernel";
arch = "arm";
os = "linux";
compression = "none";
load = <0xC20000cc>;
entry = <0xC20000cc>;
hash-1 {
algo = "sha1";
};
};
Or you can used uncomprressed kernel: "Image" (time with decompression need to be chacked)
kernel {
description = "Linux kernel";
data = /incbin/("Image");
type = "kernel";
arch = "arm";
os = "linux";
compression = "none";
load = <0xC0008000>;
entry = <0xC0008000>;
hash-1 {
algo = "sha1";
};
};
Regards
Patrick
2020-10-22 3:35 AM
Hi @Community member
Perfectly clear, thank you.
It is a pity that for option 3 (run zImage in place) one needs to manually calculate the load/entry addresses since, as you say, these addresses depend on the content of the FIT image. It would be great if mkimage had an option for this.
I agree that option 2 should be the fastest.
Thank you,
Guillermo
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.