2020-09-11 4:16 AM
hi
i am using stm32mp157caa3, there is a i2c slave operating at 3v3, while design, we have not connected( "forget")pull up line on i2c clk and data line,
so i tried enabling open-drain internal pull up in dtsi , but i2cdetect is not able to find the slave device
dtsi :
pins {
pinmux = <STM32_PINMUX('H', 11, AF5)>, /* I2C1_SCL */
<STM32_PINMUX('B', 9, AF4)>; /* I2C1_SDA */
bias-pull-up;
drive-open-drain;
slew-rate = <1>;
};
let me if my configuration and understanding is right ?
2020-09-11 6:27 AM
The internal pullup is ~50kOhm whereas the I2C bus needs ~4.7kOhm. It may work, but I would want to check the signal edges on a scope. You can also try lowering the speed.
2020-09-11 8:43 AM
Thanks, please confirm your observation, that would be helpful for validation, Mean while i will check lowering the speed and let you know.
slave is sgtl5000
but is my dtsi configuration dtsi file for internal pull up is correct ?
2020-09-11 9:23 AM
> please confirm your observation
What I'm saying is if it were my project, that's what I would be checking. That's what I'm suggesting you do.
I just realized this is not for an MCU but for an MPU (despite the tag), which I am considerably less familiar with. I still think the internal pullup is the issue.
2020-09-11 9:31 AM
4K7 is still quite high,depend on the capacitive loading, I'd lean more to 2K7 on a 3V bus. Definitely look at the rise time you're seeing on the bus, especially at the far end if the trace/wires are long. Watch grounding and current return paths.
Recently had someone run into issue on the Arduino DUE which used 1K5, which looked to be attributable to the current on the OD transistor.
2020-09-13 8:35 PM
i made clock rate 100k hz still, i2c query fails,
with pin setting as both clk, data lines as a open drain - pull up pin configuration
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.