2024-11-10 10:25 PM - edited 2024-11-11 9:48 PM
Hi ST Team,
Hi i am trying to add the x11 support for Stm32mp1, but how to setup i do not know.
* **st-example-image-x11** (with **openstlinux-x11** distro):
Image which demonstrates an example of Basic X11 usage.
* **st-example-image-xfce.bb** (with **openstlinux-x11** distro):
Image which demonstrates an example of X11 usage with XFCE as UI.
i found this line into README,
how to to this.
2024-11-15 8:28 AM
Hi,
X11 is no more directly supported, but you can emulate it from Wayland.
Please look at this link
and how to setup display for that purpose.
BR
Philippe.
2024-11-18 5:13 AM
Thanks @PPAGE.13 , this works , and I'm able to play chromium, but there is one issue, without modification on rootfs size, it works fine.
but when I try to change rootfs image size (that is 1.3 GB) then i got the error.
md@pc:~/Workspace/Kris_V4.1.2/oe-manifest/build-openstlinuxweston-stm32mp1/tmp-glibc/deploy/images/stm32mp1$ ./scripts/create_sdcard_from_flashlayout.sh ./flashlayout_st-image-core/optee/FlashLayout_sdcard_stm32mp157f-dk2-optee.tsv
Create Raw empty image: ./flashlayout_st-image-core/optee/../../FlashLayout_sdcard_stm32mp157f-dk2-optee.raw of 1536MB
Create partition table:
[CREATED] part 01: fsbl1 [partition size 256.0 KiB]
[CREATED] part 02: fsbl2 [partition size 256.0 KiB]
[CREATED] part 03: metadata1 [partition size 256.0 KiB]
[CREATED] part 04: metadata2 [partition size 256.0 KiB]
[CREATED] part 05: fip-a [partition size 4.0 MiB]
[CREATED] part 06: fip-b [partition size 4.0 MiB]
[CREATED] part 07: u-boot-env [partition size 512.0 KiB]
[CREATED] part 08: bootfs [partition size 64.0 MiB]
[CREATED] part 09: vendorfs [partition size 16.0 MiB]
[CREATED] part 10: rootfs [partition size 1.3 GiB]
!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!
[ERROR]: IMAGE TOO BIG [userfs:st-image-userfs-openstlinux-weston-stm32mp1.ext4 128 MB]
[ERROR]: There is not enough place on last partition(userfs)
then i reduce the image size only 1gb then it works and flash successful on SD card , but when i boot the image then i got the error.
[ 22.356492] ---[ end Kernel panic - not syncing: Attempted to kill init! exitcode=0x00000100 ]---
E/TC:1 Panic 'Watchdog' at ?:0
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.