2025-05-26 8:06 PM - edited 2025-05-26 8:07 PM
Hello
I am working on the multi-system in STM32MP257-EV board, I had modified the tsv file to prepare a double system A and B. If using the default metadata.bin file, the A system will be run always. Now I want the B system to be run, I need to modify the metadata.bin file, for example change the "accepted" of B bank to false:
If the status of img_0_bank_1 is trial, the B bank system will be run when ev board power up, isn't it?
how to modify the metadata.bin?
If the status of img_0_bank_1 has been modified to trial, and the B bank system run up normally, is the status of img_0_bank_1 modified automatically by linux? how does the linux system modify the metadata.bin file?
Solved! Go to Solution.
2025-05-27 12:08 AM - edited 2025-05-27 12:30 AM
Hi @longfeili_00001,
I written a wiki page which answers to your question, but it's not yet published.
I copy paste the content of the article:
The mkfwumdata tool (from U-Boot) is used to generate the metadata partition.
Metadata generation is described in the following wiki article: Metadata generation tool, nevertheless, this version of mkfwumdata doesn't support valid bank state (only accepted and invalid are supported).
So, please apply the following patch in U-Boot to bring the feature (this patch will be integrated in v6.1.0 Ecosystem Release): autoboot-propagate-boot-index.patch .
FWU metadata considers three states where two of them can correspond to Firmware update state machine:
UUID_LIST="8a7a84a0-8387-40f6-ab41-a8b9a5a60d23,19d5df83-11b0-457b-be2c-7559c13142a5,4fd84c93-54ef-463f-a7ef-ae25ff887087,09c54952-d5bf-45af-acee-335303766fb3"
OPTIONS="-g -i 1 -b 2 -v 2"
bank_state="A,V"
mkfwumdata ${OPTIONS} -s ${bank_state} -a 1 -p 0 ${UUID_LIST} /dev/disk/by-partlabel/metadata1
mkfwumdata ${OPTIONS} -s ${bank_state} -a 1 -p 0 ${UUID_LIST} /dev/disk/by-partlabel/metadata2
Don't forget to update /dev/disk/by-partlabel/metadata2 which is the backup of metadata1, and will be used by TF-A in case of CRC error of metadata1 partition.
UUID_LIST="8a7a84a0-8387-40f6-ab41-a8b9a5a60d23,19d5df83-11b0-457b-be2c-7559c13142a5,4fd84c93-54ef-463f-a7ef-ae25ff887087,09c54952-d5bf-45af-acee-335303766fb3"
OPTIONS="-g -i 1 -b 2 -v 2"
bank_state="A,A"
mkfwumdata ${OPTIONS} -s ${bank_state} -a 1 -p 0 ${UUID_LIST} /dev/disk/by-partlabel/metadata1
mkfwumdata ${OPTIONS} -s ${bank_state} -a 1 -p 0 ${UUID_LIST} /dev/disk/by-partlabel/metadata2
This can be done in a systemd service:
$ cat status-mark-good.service [Unit] Description=Good-marking Service [Service] ExecStart=/bin/bash /usr/bin/st-status-mark-good.sh [Install] WantedBy=multi-user.target
where st-status-mark-good.sh script asks the update manager to update the metadata partition to switch the bank B state to Accepted.
BR,
Christophe
2025-05-27 12:08 AM - edited 2025-05-27 12:30 AM
Hi @longfeili_00001,
I written a wiki page which answers to your question, but it's not yet published.
I copy paste the content of the article:
The mkfwumdata tool (from U-Boot) is used to generate the metadata partition.
Metadata generation is described in the following wiki article: Metadata generation tool, nevertheless, this version of mkfwumdata doesn't support valid bank state (only accepted and invalid are supported).
So, please apply the following patch in U-Boot to bring the feature (this patch will be integrated in v6.1.0 Ecosystem Release): autoboot-propagate-boot-index.patch .
FWU metadata considers three states where two of them can correspond to Firmware update state machine:
UUID_LIST="8a7a84a0-8387-40f6-ab41-a8b9a5a60d23,19d5df83-11b0-457b-be2c-7559c13142a5,4fd84c93-54ef-463f-a7ef-ae25ff887087,09c54952-d5bf-45af-acee-335303766fb3"
OPTIONS="-g -i 1 -b 2 -v 2"
bank_state="A,V"
mkfwumdata ${OPTIONS} -s ${bank_state} -a 1 -p 0 ${UUID_LIST} /dev/disk/by-partlabel/metadata1
mkfwumdata ${OPTIONS} -s ${bank_state} -a 1 -p 0 ${UUID_LIST} /dev/disk/by-partlabel/metadata2
Don't forget to update /dev/disk/by-partlabel/metadata2 which is the backup of metadata1, and will be used by TF-A in case of CRC error of metadata1 partition.
UUID_LIST="8a7a84a0-8387-40f6-ab41-a8b9a5a60d23,19d5df83-11b0-457b-be2c-7559c13142a5,4fd84c93-54ef-463f-a7ef-ae25ff887087,09c54952-d5bf-45af-acee-335303766fb3"
OPTIONS="-g -i 1 -b 2 -v 2"
bank_state="A,A"
mkfwumdata ${OPTIONS} -s ${bank_state} -a 1 -p 0 ${UUID_LIST} /dev/disk/by-partlabel/metadata1
mkfwumdata ${OPTIONS} -s ${bank_state} -a 1 -p 0 ${UUID_LIST} /dev/disk/by-partlabel/metadata2
This can be done in a systemd service:
$ cat status-mark-good.service [Unit] Description=Good-marking Service [Service] ExecStart=/bin/bash /usr/bin/st-status-mark-good.sh [Install] WantedBy=multi-user.target
where st-status-mark-good.sh script asks the update manager to update the metadata partition to switch the bank B state to Accepted.
BR,
Christophe
2025-05-27 4:32 AM
Hello Christophe
Thanks for your reply!
I had add the patch into my uboot code and rebuilt the uboot, but no new mkfwumdata tool generated. The following is the command used to build the uboot:
make -f $PWD/../Makefile.sdk DEPLOYDIR=$FIP_DEPLOYDIR_ROOT/u-boot UBOOT_CONFIG="default programmer" UBOOT_DEFCONFIG=stm32mp25_defconfig UBOOT_BINARY=u-boot.dtb DEVICE_TREE=stm32mp257f-ev1 FIP_CONFIG="optee-sdcard optee-programmer-usb" all
can this command build out the new mkfwumdata tool?
how does the mkfwumdata tool generated?
2025-05-27 5:05 AM
In configs/stm32mp25/defconfig:
CONFIG_TOOLS_MKFWUMDATA=y
Then,
make stm32mp25_defconfig
make DEVICE_TREE=stm32mp257f-ev1 all -j12
BR,
Christophe
2025-05-27 5:37 AM
hello Christophe
the new mkfwumdata tool has been generated:
./mkfwumdata --help
Usage: mkfwumdata [options] <UUIDs list> <output file>
Options:
-i, --images <num> Number of images (mandatory)
-b, --banks <num> Number of banks (mandatory)
-v, --version Metadata version (mandatory)
-s, --bank-state <val> list of bank states (default=A (accepted), V(valid) or I(invalid)
-a, --active-bank <num> Active bank (default=0)
-p, --previous-bank <num> Previous active bank (default=active_bank - 1)
-g, --guid Use GUID instead of UUID
-V, --vendor-file Vendor data file to append to the metadata
-h, --help print a help message
And regenerate the metadata.bin file use the following command:
./mkfwumdata -g -i 1 -b 2 -v 2 -s "A,V" -a 1 -p 0 8a7a84a0-8387-40f6-ab41-a8b9a5a60d23,19d5df83-11b0-457b-be2c-7559c13142a5,4fd84c93-54ef-463f-a7ef-ae25ff887087,09c54952-d5bf-45af-acee-335303766fb3 ~/metadata_tool/metadat
a.bin
Then, I use the fwumd_tool.py tool in tf-a transfer bin file to json file:
./fwumd_tool.py binparse ~/metadata_tool/metadata.bin -j ~/metadata_tool/metadata.json
Then, cat it to check if the status of bank changed or not, and it looks like the new tool not work:
cat ~/metadata_tool/metadata.json
{
"metadata": {
"crc_32": 3929930603,
"version": 2,
"active_index": 1,
"previous_active_index": 0,
"img_entry": {
"img_0": {
"location": "loc_00010002_0050_0018_83df_d519b0117b45",
"img_bank_info": {
"img_0_bank_0": {
"accepted": true,
"reserved": 588097189
},
"img_0_bank_1": {
"accepted": true,
"reserved": 0
}
}
}
}
},
2025-05-27 6:18 AM
The tool named fwumd_tool.py is only compatible with metadata v1.
The tool named mkfwumdata is only compatible with metadata v2.
Here, you used fwumd_tool.py with metadata v2.
To check if the metadata is well built with mkfwumdata, write the generated file into metadata partitions, are reboot the platform to check the impact in TF-A.
BR,
Christophe
2025-05-27 7:21 PM
Hello
Thanks very much, it looks work well.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.