2022-09-22 7:10 AM
Hello All,
We have the STM32MP1xxx-DK. and we had build the image for this board using the steps mentioned on ST wiki to generate the distribution image.
We had build st-image-core as its size is less then Weston image.
We want not to enable the SPI-5 so that we can done some testing on SPI.
Can you please guide us where we need to do changes to enable the spi.
We are new in Linux.
Thanks
2022-10-10 1:04 AM
Hi @HVerm.3,
You have to enable the SPI-5 instance in DeviceTree board level. (likely using CubeMX)
Please check-out following links :
STM32 MPU device tree - stm32mpu
SPI internal peripheral - stm32mpu
SPI device tree configuration - stm32mpu
Hope it help,
Olivier
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.