2020-07-23 10:54 AM
Hello,
We are considering the STM32MP151x MPU for a new project. However we need at least 20 independent PWM outputs (at the same frequency but different duty cycle). After reading the datasheet, it is still not clear to me how many PWMs STM32MP151x has.
TIM1, TIM8 ==> 2 x 6 independent channels (at the same frequency) ?
TIM2, TIM3, TIM4, TIM5 ==> 4 independent channels ?
TIM13, TIM14, TIM16, TIM17 ==> 4 independent channels ?
TIM12, TIM15 ==> 4 independent channels ?
Total 24, am I right ?
Thanks
Hugo
2020-07-24 12:13 AM
Hello,
according to Datasheet table "Timer feature comparison", here is my slightly different count:
TIM1 and TIM8 = 4 channels each
TIM2, TIM3, TIM4 and TIM5 = 4 channels each
TIM12 and TIM15 = 2 channels each
TIM13, TIM14, TIM16 and TIM17 = 1 channel each
LPTIM1, LPTIM2, LPTIM3, LPTIM4 and LPTIM5, although not having capture channel, get a compare, so can do PWM too.
Total: 37 channels
BUT, you should check using CubeMX that all those pins (TIMx_CHy or LPTIM_OUT) could be output on distinct pins according to your specific application constrains (e.g. at least the required boot Flash interface).
Note that if some TIMx_CHy are not available, TIMx_CHyN could be used instead (complementary channel not available on all channels).
Regards.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.