2021-04-08 7:24 AM
Hello,
I would like to enable battery/capacitor charging from the VBAT pin on an STM32MP1 and also change the charging resistor.
That would be VBE and VBRS of PWR_CR3.
What would be the proper way to enable/disable the charging together with the resistor value from Linux and/or U-boot?
The regulator driver managing PWR_CR3 does not mention VBE or VBRS.
Thanks
2021-04-28 8:45 AM
Hi,
I think for the moment, these bits are not managed by Device Tree, you could probably modify TF-A for that specific purpose.
Regards.
2021-08-04 12:38 AM
Hello,
A change request is under discussion in ST to implement it in Device tree. For ST this would be required only in TF-A but would you really need to enable the register settings in u-boot or Linux (or TF-a is enough for your need) ?
2021-08-04 1:14 AM
I missed the reply button. See above.
(Unable to delete)
2021-08-04 1:14 AM
Great thanks!
Currently I enable the setting in U-Boot, but any stage is fine (TF-A, U-Boot or Linux) . TF-A would work perfectly fine.
Again thanks!
2021-08-04 4:45 AM
Ok thanks for the quick answer.
fyi, in tf-a and optee the function "raw_allowed_access_request()" allows to set these bits.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.