cancel
Showing results for 
Search instead for 
Did you mean: 

Custom DTS Overlay Memory Reservation Not Reflected After Boot on STM32MP157F-DK2

VedantK33
Associate II

Hi everyone,

I am trying to reserve a block of RAM using a custom device tree overlay on my STM32MP157F-DK2 running Linux. Here's what I have done so far:

This is my custom DTS overlay

/dts-v1/;
/plugin/;
/ {
    compatible = "st,stm32mp157f-dk2", "st,stm32mp157";
    fragment@0 {
        target-path = "/reserved-memory";
        __overlay__ {
            sensor_shm: sensor_shm@c8000000 {
                compatible = "shared-dma-pool";
                reg = <0xc8000000 0x00040000>; /* 256KB */
                no-map;
                status = "okay";
            };
        };
    };
};

 

I compiled this to get custom-overlay.dtbo and placed it under /boot/overlays/.

Then, I edited the /boot/mmc0_extlinux/stm32mp157f-dk2_extlinux.conf configuration file to include the overlay during boot by adding this line inside the appropriate boot label:

 

# Generic Distro Configuration file generated by OpenEmbedded
menu title Select the boot mode
MENU BACKGROUND /splash_portrait.bmp
TIMEOUT 20
DEFAULT OpenSTLinux
LABEL OpenSTLinux
        KERNEL /uImage
        FDTDIR /
        INITRD /st-image-resize-initrd
        APPEND root=PARTUUID=e91c4e10-16e6-4c0e-bd0e-77becf4a3582 rootwait rw   console=${console},${baudrate}
        fdtoverlays /boot/overlays/custom-overlay.dtbo
LABEL stm32mp157f-dk2-a7-examples
        KERNEL /uImage
        FDT /stm32mp157f-dk2-a7-examples.dtb
        INITRD /st-image-resize-initrd
        APPEND root=PARTUUID=e91c4e10-16e6-4c0e-bd0e-77becf4a3582 rootwait rw   console=${console},${baudrate}
LABEL stm32mp157f-dk2-m4-examples
        KERNEL /uImage
        FDT /stm32mp157f-dk2-m4-examples.dtb
        INITRD /st-image-resize-initrd
        APPEND root=PARTUUID=e91c4e10-16e6-4c0e-bd0e-77becf4a3582 rootwait rw   console=${console},${baudrate}
~

Problem:
After reboot, the reserved memory node /reserved-memory/sensor_shm does not appear in the device tree (checked via /proc/device-tree), and my memory reservation does not take effect.

Could someone please help me identify what I might be missing or doing wrong with the overlay or boot configuration?

Thank you!

1 ACCEPTED SOLUTION

Accepted Solutions

Hello @VedantK33 ,
If you built the default OpenSTLinux distribution as explained in the wiki, so the default U-Boot configuration might not have CONFIG_OF_LIBFDT_OVERLAY configured by default, regarding the stm32mp15_defconfig file in sources of U-Boot.

You have 2 different options:

  • Creating a patch for U-Boot that modify the stm32mp15_defconfig and add the necessary configuration. Then add this patch as a bbappend in your Yocto build
  • Cross compiling out of Yocto U-Boot with the modified configuration, and deploy it in your FIP used on your target (what we call the Developer Package method)

Kind regards,
Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

4 REPLIES 4
Erwan SZYMANSKI
ST Employee

Hello @VedantK33 ,
Few investigations path you can check at:

  • Does your U-Boot has the necessary configuration to support DTBO ? I think we disable it by default for security reason, but need to double check. The config seems to be CONFIG_LIBFDT_OVERLAY
  • Check if caps are not mandatory in your extconf file read by U-Boot. We have this example for X-LINUXTSNSWCH as extconf U-Boot file:
  • LABEL stm32mp257f-ev1-tsn
            KERNEL /Image.gz
            FDTDIR /
            FDTOVERLAYS /devicetree/stm32mp25xx-ev1-swch.dtbo
            INITRD /st-image-resize-initrd
            APPEND root=PARTUUID=e91c4e10-16e6-4c0e-bd0e-77becf4a3582 rootwait rw   earlycon console=${console},${baudrate}
    
  • Add logs in U-Boot in pxe_utils.c file to check if the overlay is well detected and applied.

Kind regards,
Erwan. 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

How can I check my U-boot configuration ? I think I cant change it as the configuration file is baked at build time and now what we have on board is U-boot binary. So I might have to build U-boot with desired configuration. Please correct me if I am wrong. 

Hello @VedantK33 ,
If you built the default OpenSTLinux distribution as explained in the wiki, so the default U-Boot configuration might not have CONFIG_OF_LIBFDT_OVERLAY configured by default, regarding the stm32mp15_defconfig file in sources of U-Boot.

You have 2 different options:

  • Creating a patch for U-Boot that modify the stm32mp15_defconfig and add the necessary configuration. Then add this patch as a bbappend in your Yocto build
  • Cross compiling out of Yocto U-Boot with the modified configuration, and deploy it in your FIP used on your target (what we call the Developer Package method)

Kind regards,
Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Hey @Erwan SZYMANSKI 

Thanks for replying.

I used another way to overlay custom-overlay on the stm32mp157f.dts file. 

It is very simple and does not require developer package method.

I am pasting link below where I have mentioned steps to create reserved memory 

Guide to create reserved memory 

Thanks and regards,

Vedant.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.