2022-08-19 11:25 AM
Hello ,
Can anyone please point me to the example of SPI communication between stm32(F4/L0/L4) with A7 of STM32MP1?
A7 could be a driver or any user application but both should be able to send and receive the data over spi.
on A7 I suppose it will be SPI5.
please assist.
Thanks in advance!
Br,,
P
2022-09-01 6:02 AM
Hi @PVaaz.1
is those pages help you for a start point ?
https://wiki.st.com/stm32mpu/wiki/SPI_overview#API_description
https://wiki.st.com/stm32mpu/wiki/How_to_use_SPI_from_Linux_userland_with_spidev
Regards
In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.