2024-11-10 11:34 PM
Hi,
I am unable to see the can0/can1 interface on my brand new STM32MP2 Eval board after re-flashing the Starter-Package(FlashLayout_sdcard_stm32mp257f-ev1-ca35tdcid-ostl-m33-examples-optee.tsv).
Previously I was able to see both the interfaces(with ls /sys/class/net) with the preloaded micro-sdcard OS that came with the board and was able to send/receive CAN data to external devices.
But after flashing the firmware that came with starter-package: stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26, CAN interface stopped working. I tried modprobe the can driver and also rebuilding/flashing the kernel/DTS using the Developer package but nothing helps.
Unfortunately I didn't backup the micro-sd contents before reflashing. I assumed the sdcard was loaded with starter-package contents when the board arrived.
Any help would be highly appreciated.
Thanks,
Satish
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.