2020-05-27 5:59 PM
I'm trying to figure out how to add OpenCV to my STM32MP157-DK2 Discovery Board. I am not new to ST Microcontrollers, but I am new to the MP1 and Cortex A processors. I'm also not new to Linux but am completely new to embedded Linux and Yocto.
I can see that there is a recipe for OpenCV included in the Ecosystem V1.2 release distribution package, but when I build the release and flash, OpenCV is not present on the DK2 board. I was able build OpenCV specifically with the bitbake command, but again, it is not present in the image. I have seen a few references to installing OpenCV in the wiki but not enough details to get to the next step.
I am wondering what the correct or preferred method for getting OpenCV included in the image. Preferably, enough information or pointers to documentation that I can understand the bigger picture and know how to do this in general and not simply how just to add OpenCV in this case.
2020-05-27 11:37 PM
Hello @Community member ,
If you want to add a recipe into your image, you need to add this recipe in the image recipe (st-image-weston.bb if you build this image)
Feel free to look into the wiki.
BR,
Christophe
2020-06-01 12:47 AM
Hello @Community member ,
you can also use apt-get mechanism to install on board required packages/libraries.
See article https://wiki.st.com/stm32mpu/wiki/Package_repository_for_OpenSTLinux_distribution
Board $> apt-get update
Board $> apt-cache search opencv
I believe you will find the one you need.
BR,
Milan
2022-04-28 7:17 PM
Hello DRuss, I want to know if you have solved this question. cause I also need to add OpenCV to my MP1 board. Look forwward your reply!
2022-04-29 4:00 AM
I abandoned developing for the MP1 board long ago, so there is not much I remember or can help you with. The answer I ultimately came up with was to add my own layer to yocto and rebuild. The layer brought in OpenCV. I'll paste my notes below, but I have to admit that they don't make much sense to me now. If they don't make sense to you then, I apologize, but there is not much I can do at this point. I know this worked and that we were able to run OpenCV, but we did not get the performance that we needed and moved onto other things (and other projects).
- https://wiki.st.com/stm32mpu/wiki/How_to_create_your_own_image
- https://wiki.st.com/stm32mpu/wiki/How_to_create_a_new_open_embedded_layer
- First, create a new layer.
- source your BitBake enve setup
- cd STM32MPU_workspace/STM32MP15-Ecosystem-v1.2.0/Distribution_Package/openstlinux-20-02-19
- source ./layers/meta-st/scripts/envsetup.sh
- Get a list of existing layers
- bitbake-layers show-layers
- Create the new layer
- Specify:
- Location of the new layer
- Name of the new layer
- (Optionally) the priority of the new layer
- bitbake-layers create-layer ../layers/meta-foo/meta-foo-image
- Add the new layer to your configuration
- bitbake-layers add-layer../layers/meta-foo/meta-foo-image
- Add a recipe for the image
- cd ../layers/meta-foo/meta-foo-images
- mkdir recipes-foo
- cd recipes-foo
- mkdir images
- cd images
- touch foo-image-weston.bb
- gedit foo-image-weston.bb
- Add the following to the file
require recipes-st/images/st-image-weston.bb
SUMMARY = "Image modified for FOO"
#
# INSTALL addons
# Note - Yocto documentation says that using CORE_IMAGE_EXTRA_INSTALL here
# is incorrect and that this variable should only be used in local.conf.
#
CORE_IMAGE_EXTRA_INSTALL += " \
opencv \
"
- Save and exit gedit
- Build Image
- bitbake foo-image-weston
- Flash Image
- Out of Scope for this document
- Generate SDK
- bitbake -c populate_sdk foo-image-weston
- Generate Extended SDK
- bitbake -c populate_sdk_ext foo-image-weston
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.