on
2025-05-20
7:00 AM
- edited on
2025-11-26
5:28 AM
by
Laurids_PETERSE
Understanding the absolute maximum ratings of STM32 microcontrollers (MCUs) is critical for ensuring their reliability and longevity. These ratings define the limits beyond which the device may suffer permanent damage. This article explores the significance of these ratings and the potential impacts of exceeding them.
The absolute maximum ratings values for STM32 MCUs provide voltage, current, and thermal characteristics. These ratings are stress limits, and functional operation of the device in these conditions is not implied. Prolonged exposure to these conditions can affect the device's reliability and may lead to permanent damage.
The absolute maximum ratings are presented in the STM32 datasheet precisely in the “Absolute maximum ratings” section. This section provides the absolute maximum rating values for the voltage, current, and thermal.
You can find below an example of absolute maximum ratings values for STM32U575 mentioned in DS13737.
We acknowledge that the product is not damaged until AMR (absolute maximum ratings) values are reached. These limits are valid for all devices, considering spread and variations in the manufacturing process. It is recommended to avoid levels above absolute maximum ratings. Ensure that the STM32 MCU is functioning in accordance with the operating conditions shared in the datasheet in the "Operating conditions" section.
Above the absolute maximum rating the device may still work, but the functionality is not warranted. Make sure that the STM32 MCU does not operate above the maximum ratings.
Of course, this isn't specific to STM32 - or even to ST.
This is an industry-wide understanding of the term, "Absolute Maximum Ratings".
The final paragraph seems to have lost something in translation:
@KDJEM.1 wrote:Above absolute maximum ratings, conditions do not allow admitted (sic?) the sample operation and integrity anymore.
Should "admitted" be "ST to guarantee" ?
There is a probability that samples can handle such conditions without any estimation
Pardon?
Hello @Andrew Neil;
Thank you for your feedback.
Some adjustments have been made to improve clarity.
Kaouthar
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.