on
2021-06-23
2:22 AM
- edited on
2025-12-04
6:44 AM
by
Laurids_PETERSE
The STM32H7 products are part of the most powerful STM32 and bring many new features and capabilities. The drawback is the increase of the complexity of the system. Many resources are available on the ST community but also on the net to help you. The purpose of this article is listing the most useful resources.
The STM32H7 products are part of the most powerful STM32 and bring many new features and capabilities. The drawback is the increase of the complexity of the system. Many resources are available on the ST community but also on the web to help you.
The purpose of this article is to list the most useful resources:
This article explains the memory layout of the platform and the cache that have an impact on the DMA usage.
DMA-is-not-working-on-STM32H7-devices
This article explains you step by step how to create a basic example on a STM32H750-Discovery (but this could be re-used for other board).
How-to-create-project-for-STM32H7-with-Ethernet-and-LwIP-stack-working
Ethernet-not-working-on-STM32H7x3
This article explains the potential issue with buffer location and cache issue. Additionally, it will provide you an example with STM32H743I-EVAL, STM32CubeMX, & STM32CubeIDE.
How-to-enable-dma-in-usb-with-stm32h7-devices
This article points out two possible issues: power supply misconfiguration and Cortex-M7 boot disabled (for dual core config).
Unable-to-connect-to-STM32H7-devices
This MOOC shows the MPU usage in STM32 with ARM CortexM7. This will allow you to understand the Memory Protection Unit (MPU) with CortexM7 based. You will be able to perform MPU setting examples on STM32F7 / STM32H7 devices.
MOOC-STM32_MPU_tips
This article explains you the root cause of this issue and how to solve it.
FAQ: STM32 SRAM/Backup SRAM content is not preserved after reset
This MOOC explains step by step how to create an external loader. Example is based on STM32F7 but still relevant for STM32H7.
MOOC-External_QSPI_loader_creation
This article explains how to find out this state and how to configure it
Default-state-of-stm32h7-switches-connecting-pxy-c-and-pxy-pads
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.