cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 MCU errata sheets: Expected preliminary updates

KDJEM.1
ST Employee

Introduction

This article includes preliminary updates of STM32 MCU errata sheets reported since 1st January 2024It highlights the current description requiring update and the expected one if available.

The purpose of this article is to deliver any expected updates to our MCU errata sheets prior to actual documentation releases. We wish to be transparent with our updates and provide them as fast as possible, to assist you in your design process.
This article is updated on a quarterly basis. Once these preliminary updates are manifested in the errata sheets, this article is refreshed with new information.
Moving forward, we are also working on providing errata sheet releases on a more frequent basis.

IMPORTANT NOTICE - READ CAREFULLY:

  • STMicroelectronics NV and its subsidiaries (“ST”) reserve the right to make changes, corrections, enhancements, modifications, and improvements to this article at any time without notice.
  • Information in this article supersedes and replaces information previously supplied in any prior versions of this article.
  • The following table gives a quick reference to the preliminary documentation updates which may be changed or improved without notice.
  • This article will be reviewed on a quarterly basis and applied updates will be removed from the table.
  • The hyperlinks under "Doc Reference - Revision" provides a direct link to the specific document page where the description is located.

Summary of documentation updates: "STM32 MCU errata sheets"

Function Series/Lines Doc Reference - Revision Description Date of added update
SPI

STM32F427xx

STM32F437xx

STM32F429xx

STM32F439xx

ES0206 Rev23

(Feb 2025)

Add section: 

Corrupted last bit of data and/or CRC, received in Master mode with delayed SCK feedback

Description
When performing a receive transaction in I2S or SPI Master mode, the last bit of the transacted frame is not captured when the signal provided by an internal feedback loop from the SCK pin exceeds a critical delay. The lastly transacted bit of the stored data then keeps the value from the pattern received previously. As a consequence, the last receive data bit may be wrong, and/or the CRCERR flag can be unduly asserted in the SPI mode if any data under checksum, and/or just the CRC pattern is wrongly captured. In SPI mode, data are synchronous with the APB clock. A delay of up to two APB clock periods can thus be tolerated for the internal feedback delay. The I2S mode is more sensitive than the SPI mode, especially in the case where an odd I2S prescaler factor is set and the APB clock is the system clock divided by two. In this case, the internal feedback delay is lower than 1.5 APB clock period. The main factors contributing to the delay increase are low VDD level, high temperature, high SCK pin capacitive load, and low SCK I/O output speed. The SPI communication speed has no impact.

Workaround
The following workarounds can be adopted, jointly or individually:
• Decrease the APB clock speed.
• Configure the I/O pad of the SCK pin to be faster.
The following table gives the maximum allowable APB frequency (that still prevents the issue from occurring) versus GPIOx_OSPEEDR output speed for the SCK pin, with a 30 pF capacitive load.

KDJEM1_1-1712142798747.png

 

Mar 2024


 

System

STM32G471xx
STM32G473xx
STM32G474xx
STM32G483xx
STM32G484xx

ES0430 Rev9

(Jun 2024)

Remove section:

The same errata looks to appear 2 times :

2.2.5 MCU cannot enter in Standby mode when HSE bypass used
2.2.10 Device cannot enter Standby mode when HSE bypass used as system clock

Jun 2025

STM32H503CB
STM32H503EB
STM32H503KB
STM32H503RB

ES0561 Rev5
(Dec 2025)

Current:

Debug authentication services unavailable after direct transition from OPEN to CLOSED

Description
Debug authentication (DA) services fail and debug access through DA is not available if the device is provisioned
using the following sequence:
1. The product is in VIRGIN state (never used).
2. A provisioning firmware is downloaded and executed while the device is in PRODUCT_STATE = OPEN.
This firmware:––
Programs the OTP for debug authentication, and
Directly sets PRODUCT_STATE = CLOSED.
No external programmer is used to transition the device from PRODUCT_STATE = PROVISIONING to
PRODUCT_STATE = CLOSED.
As a result, the internal debug authentication configuration is not correctly established, and DA services cannot be
used.
Workaround
1. Using a firmware:
a. Download a first firmware whose only purpose is to set PRODUCT_STATE = REGRESSION.
b. After this first firmware has run successfully, change the product state to
PRODUCT_STATE = IROT‑PROVISIONED.
c. Reset the device to execute the regression process.
2. Executing the system bootloader:
a. While the device is in PRODUCT_STATE = OPEN, set the BOOT0 pin to VDD.
3. Perform a debug authentication discovery procedure via the bootloader.
4. Provision the product using PRODUCT_STATE = PROVISIONING, and then follow the standard provisioning
flow.

Expected:

Debug Authentication fails if change of PRODUCT_STATE is done by embedded firmware

Description

Debug authentication (DA) services fail and regression through DA is not available if the device is provisioned using the following sequence: 
The product is in VIRGIN state (never used). 
The firmware is downloaded and executed while the device is in PRODUCT_STATE = Open. 
This firmware programs the OTP for debug authentication, and changes PRODUCT_STATE to iROT-Provisioned or Closed.
Note: new PRODUCT_STATE is active after changing option byte change followed by a system reset. Firmware can go from Open to Closed through iROT-Provisioning or Provisioned states by changing twice the PRODUCT_STATE and finishing by a system reset.
Workaround
On a virgin device before flashing the embedded firmware that changes the PRODUCT_STATE
Go though a regression triggered by a dedicated firmware
Program the dedicated firmware
Dedicated firmware detects Open state : changes PRODUCT_STATE to Provisioned and resets
Dedicated firmware detects Provisioned state : changed PRODUCT_STATE to Regression and resets
Set BOOT0 pin to VDD and reset the target. Set back BOOT0 to VSS Launch DA discovery in Open state and reset the target

Mar 2026

IWDG

STM32F100x4 STM32F100x6
STM32F100x8 STM32F100xB

ES093 Rev8

(Jul 2022)

Remove sections:

Delete duplicated sections:

- RVU flag not cleared at low APB clock frequency

- PVU flag not cleared at low APB clock frequency

Mar
2024

STM32F10xx4 STM32F10xx6

ES0348 Rev10

(Jun 2022)

STM32F101xF
STM32F101xG STM32F103xF
STM32F103xG 

ES0346 Rev7

(Jul 2022)

STM32F101xC
STM32F101xD
STM32F101xE
STM32F103xC
STM32F103xD
STM32F103xE

ES0340 Rev17

(Jun 2022)

STM32F105xx STM32F107xx

ES022 Rev11

(Jun 2022)

STM32F100xC
STM32F100xD STM32F100xE

ES0136 Rev7

(Aug 2022)

HRTIM

STM32F334x4
STM32F334x6
STM32F334x8

ES0258 Rev8

(Aug 2021)

Table 4. Summary of silicon limitations

Current:

KDJEM1_0-1733228672726.png

A = limitation present, workaround available

Expected:KDJEM1_1-1733228771070.png

With N = limitation present, no workaround available

Nov 2024

ADC

STM32L412xx
STM32L422xB

ES0456 Rev6 (Nov 2024)

Remove section:

Delete duplicated section:

"2.6.9 Writing ADCx_JSQR when JADCSTART and JQDIS are set might lead to incorrect behavior" should be removed. It is duplicated with "2.6.1 Writing ADC_JSQR when JADCSTART and JQDIS are set may lead to incorrect behavior"

Dec 2024
CEC

STM32H7A3xI STM32H7A3xG
STM32H7B0xB STM32H7B3xI

ES0478 Rev11 (Apr 2022)

Add section:

Unexpected TXERR flag during a message transmission.

Description 

During the transmission of a 0 or a 1, the HDMI-CEC drives the open-drain output to high-Z, so that the external pull-up implements a voltage rising ramp on the CEC line.
In some load conditions, with several powered-off devices connected to the HDMI-CEC line, the rising voltage may not drive the HDMI-CEC GPIO input buffer to VIH within two HDMI-CEC clock cycles from the high-Z activation to TXERR flag assertion.
Workaround
Limit the maximum number of devices connected to the HDMI-CEC line to ensure the GPIO VIH threshold is reached within a time of two HDMI-CEC clock cycles (~61 µs).
The maximum equivalent 10%-90% rise time for the HDMI CEC line is 111.5 µs, considering a VIH threshold equal to 0.7 x VDD.

Dec 2024
OCTOSPI

STM32H7A3xI STM32H7A3xG
STM32H7B0xB STM32H7B3xI

ES0478 Rev11 (Apr 2022)

Add section:

Transactions are limited to 8 Mbytes in OctaRAM™ memories.

Description 

When the controller is configured in Macronix OctaRAM™ mode, by setting the MTYP[2:0] bitfield of the OCTOSPI_DCR1 register to 011, only 13 bits of row address are decoded and sent to the memory, meaning that only 8 K of 1-Kbyte blocks can be accessed (8 Mbytes).
Workaround
None.
This limitation is not present for PSRAMs or HyperRAM™ memories.

Dec 2024
Applicability

STM32H7A3xI STM32H7A3xG STM32H7B0xB STM32H7B3xI

ES0478 Rev11

(Apr 2022)

Table 1. Device summary

Add:

STM32H7A3LG in the part numbers list.

Jun 2025

STM32U375xx STM32U385xx

ES0626 Rev2

(Jan 2026)

Current:

2. REV_ID[5:0] bitfield of DBGMCU_IDCODE fuse

Expected:

2. REV_ID[15:0] bitfield of DBGMCU_IDCODE fuse

Dec 2025

 

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.

Version history
Last update:
‎2026-04-01 6:04 AM
Updated by:
Contributors