on
2021-05-18
9:50 AM
- edited on
2025-11-25
1:35 AM
by
Laurids_PETERSE
What are the most important information to know about LoRa communication?
What are the resources offered by ST and dedicated to the development of LoRa solutions?
This FAQ concerns the LoRa communication, this tutorial contains the basic information to know about LoRa Technology and several helpful links to get started with, based on STM32 products.
LoRa is a wireless communication technology, it is developed to create low-power, wide-area networks (LPWANs) required for machine-to-machine and IoT applications connecting many devices.
LoRa is a long-range transmission technology for higher than 10 Km and characterized by its low power consumption and its:
Note:It is important to highlight that the range LoRa transmits for is affected by multiple factors which are mainly the network used, the node-gateway positioning, the antenna, the environment… |
LoRaWAN is a global Low Power Wide Area Network (LPWAN) specification providing bi-directional communications which allows connection of LoRa devices to the internet.
LoRaWAN differs from LoRa by the inclusion of a physical layer. It consists of several elements:
Regarding the LoRa modulation characteristics, they are defined for each region and specified in the LoRaWAN Regional Parameters document, from the LoRa Alliance.
LoRa is a Sub-GHz wireless technology enabling low data rate communication over long distances so, yes, it is possible we can send data via lora protocol to another device and control it remotely.
In order to maximize the range, it is possible to:
Deploying the LoRaWAN network has several advantages presented below:
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.