cancel
Showing results for 
Search instead for 
Did you mean: 

SUBSTITUTION LORA GATEWAY WITH A STM32-L476RG

vaianallen
Associate

Hi everyone, i would create a LoRaWAN project in which both end-node and gateway are implemented by a NUCLEO-l476rg, because i haven't a gateway. The fictitous gateway is connected locally, with UART, to a python app on my pc, to handle the information trasmetted by the endnode. I have implemented both sides: 1) endnode, with a LoRaWAN endnode example from STM32CubeExpansion_LRWAN, 2) the gateway's programm is a modificated pingping example, to receive and forward then to python. 
My problem is: premising that I set the tx frequency always to the first channel(868100000) when the end-node transmit, the "gateway doesn't receive every time, as well as is showed in this log:


16s627:Packet received
26s627:Packet received
36s627:Packet received
56s627:Packet received
66s627:Packet received
96s627:Packet received
106s627:Packet received

 

The gateway should receive a packet every 10 s, but this doesn't happend. Someone can tell my why?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
STTwo-32
ST Employee

Hello @vaianallen 

I think that this is due to the different reasons. It may be due to an interference, Problems in lora Module, Long distance,...

I suggest you test such an application using the STM32WL Board For better quality.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.