2024-08-29 11:50 PM
I'm working on a project with the STM32WL55JC microcontroller. Before testing the LoRaWAN_FUOTA_DualCore application, my LoRaWAN setup was functioning correctly with all example applications.
However, after flashing the LoRaWAN_FUOTA_DualCore application, I noticed that only this application is working. While other applications like LoRaWAN_FUOTA, LoRaWAN_End_Node, and LoRaWAN_End_Node_DualCore are functional in terms of peripherals, my device is unable to connect to the LoRa gateway.
Could you help me understand why it’s only working with the LoRaWAN_FUOTA_DualCore application?
2024-10-14 8:35 AM
Hello @karthiksb
I'm not able to reproduce that issue. Could you please tell me how you have reproduced that.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.