2025-04-01 1:01 PM
Hi,
The specifications mention multi-protocol support for 4-(G)FSK, 2-(G)FSK, (G)MSK, DBPSK, DSSS, and ASK. However, the reference manual does not explicitly mention GMSK.
Can the device demodulate GMSK directly through register settings, or is it only possible via raw IQ data and external software processing?
Best Regards
Arne
Solved! Go to Solution.
2025-04-02 8:25 AM
Hello @bobbe
You can use simple 2GFSK modulation, with the difference that you need to select a modulation index of 0.5. Therefore, you should set the proper data rate and frequency deviation.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-04-02 8:25 AM
Hello @bobbe
You can use simple 2GFSK modulation, with the difference that you need to select a modulation index of 0.5. Therefore, you should set the proper data rate and frequency deviation.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.