2023-11-16 12:10 AM - edited 2023-11-16 12:55 AM
Hi,
Has someone made a FUOTA session succesful in EU868 using the Nucleo-WL55JC using FW_WL_V1.3.0?
When I run the FUOTA example, single core, the device goes to the HardFault_Handler interrupt.
This happens right after the device switches from class A to class C at the start of the FUOTA campaign. At the reception of the first frame, the device halts. The last thing I see in the serial terminal is:
###### ========== MCPS-Confirm =============
###### U/L FRAME:0070 | PORT:2 | DR:5 | PWR:7 | MSG TYPE:UNCONFIRMED
1700119218s532:RX_C on freq 869525000 Hz at DR 3
Switch to Class C done
1700119219s243:MAC rxDone
1700119219s248:BufferRX Port: 201
I have tried with DR_0 and DR_3 as downlink datarates. For DR_0 I use a maximum packet size of 48B and 112B for the DR_3.
2023-11-16 3:06 AM - edited 2023-11-16 3:09 AM
Hello @jmmunoz
In FUOTA procedure:
A bad memory access (wrong section, memory protect unit enabled on the wrong region, a non-8bytes aligned fragment) may be the cause of this error.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-11-16 4:45 AM
Hi @STTwo-32 ,
thank you for your inputs.
Reading the AN5554 document, I see that by using
#define SECBOOT_DISABLE_SECURITY_IPS /*!< Disable all security IPs at once when activated */in app_sfu.h, the security is deactivated. Is there any other security to be disable?
If I understood correctly, in the single core LoRaWAN_FUOTA there is not SBSFU.
For the second check, I haven't touched any configuration in the memory and region for storage/fragments. What should I look for?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.