cancel
Showing results for 
Search instead for 
Did you mean: 

STM32WB5MMG6 BLE_LLD works at 3.3V but not at 1.8V

jpepv
Associate II

I'm currently testing the BLE_LLD examples provided by st. I have two Nucleo Boards one running BLE_LLD_Lowpower and one running the BLE_LLD_Pressbutton example. That example works fine and I can change whatever is transmitted.

If I use the same BLE_LLD_Lowpower example on one of my own PCBs with a STM32WB5MMG6  module I can only make the example work if I provide 3.3V. If I change the supply voltage to anything else than 3.3V it only transmits one package. But as soon as it enters the LL_PWR_MODE_STOP2 low power mode and wakes up from it, it seems to be stuck at some point. If I debug said example at 1.8V it keeps on running. (I think it won't go into sleep mode).

If I run both examples unchanged and run the Lowpower example at 1.8V I get the same results.

Is there an explanation for said behaviour? Any help appreciated

1 ACCEPTED SOLUTION

Accepted Solutions
jpepv
Associate II

If I change the sendStart() to this, it works

static void sendStart(void)
{
  APP_BLE_LLD_Init();
  HW_TS_Create(CFG_TIM_PROC_ID_ISR, &SwitchOffGPIO_timer_Id, hw_ts_SingleShot, Appli_TS_Callback);

  radioInit();
  HW_TS_Start(SwitchOffGPIO_timer_Id, (uint32_t)LED_ON_TIMER);
  UTIL_LPM_SetStopMode(1 << CFG_LPM_APP_BLE_LLD, UTIL_LPM_DISABLE ); // TO ENABLE
  BLE_LLD_MakeActionPacketPending(&apSend[APACKET_1]);
}

View solution in original post

3 REPLIES 3
jpepv
Associate II

Ok, further investigation shows, that its not stuck. The example transmits 3 ActionPackets and only if all 3 are sent successful, the MCU goes to sleep. Otherwise it seems stuck. (I'm logging the current consumption)
If I recall the BLE_LLD_Init() after the first sleep, I get atleast one more packet. Then it seems stuck again.

I will investigate further

jpepv
Associate II

If I change the sendStart() to this, it works

static void sendStart(void)
{
  APP_BLE_LLD_Init();
  HW_TS_Create(CFG_TIM_PROC_ID_ISR, &SwitchOffGPIO_timer_Id, hw_ts_SingleShot, Appli_TS_Callback);

  radioInit();
  HW_TS_Start(SwitchOffGPIO_timer_Id, (uint32_t)LED_ON_TIMER);
  UTIL_LPM_SetStopMode(1 << CFG_LPM_APP_BLE_LLD, UTIL_LPM_DISABLE ); // TO ENABLE
  BLE_LLD_MakeActionPacketPending(&apSend[APACKET_1]);
}
Severex
Associate

Does anybody tried BLE_LLD_pressbutton on STM32WB15?
It works fine on WB55 but not any response on WB15

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.