2025-01-28 3:58 AM - edited 2025-01-28 4:03 AM
Hi,
Made a prototype board with a STM32WB55RGV. For testing the wake up I reduced to only UART1, incoming SYS WAKEUP PIN 4 (PA2), control LED on PB10, Serial Wire debugging. HSE/LSE present, but not used. BLE is not used, the firmware deleted, etc.
If I test by HAL_GPIO_ReadPin I can clearly detect Vcc on the Wake up pin (configured then as input) while pressing the button connected to this pin. Loosening falls down to 0/GND. A multimeter confirms 3.1V while pressing, 0V while loosening the button / in rest.
Just a simple code:
if (__HAL_PWR_GET_FLAG(PWR_FLAG_SB) != RESET)
{
__HAL_PWR_CLEAR_FLAG(PWR_FLAG_SB);
}
HAL_PWR_DisableWakeUpPin(PWR_WAKEUP_PIN4);
HAL_Delay(1000);
HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN4_HIGH);
__HAL_PWR_CLEAR_FLAG(PWR_FLAG_WU);
HAL_PWR_EnterSTANDBYMode();
The device reaches standby mode, I notice the debugger lost contact after some seconds, pretty normal I guess. While pressing the button, confirming high level on PA2/SysWakeUp4 nothing happens. If I remove power and reapply, the program is just running until the enter standby function call. An LED confirms the start of the program.
I'm lost. Also changing PWR_WAKEUP_PIN4_HIGH to _LOW or the regular doesn't change the outcome. What am I missing here?
Solved! Go to Solution.
2025-01-28 7:31 AM - edited 2025-01-28 7:32 AM
Hi,
Here is a code that worked for me (tested on an stm32wb15cc), based on the PWR_STANDBY_RTC example :
if( (LL_PWR_IsActiveFlag_C1SB() == 0)
|| (LL_PWR_IsActiveFlag_C2SB() == 0)
)
{
/* Set the lowest low-power mode for CPU2: shutdown mode */
LL_C2_PWR_SetPowerMode(LL_PWR_MODE_SHUTDOWN);
}
/* Enable pull down on wakeup pin PA2 */
LL_PWR_EnableGPIOPullDown(LL_PWR_GPIO_A, LL_PWR_GPIO_BIT_2);
/* Enable pull-up and pull-down configuration for CPU1 */
LL_PWR_EnablePUPDCfg();
/* Set wakeup pin polarity */
LL_PWR_SetWakeUpPinPolarityHigh(LL_PWR_WAKEUP_PIN4);
/* Enable wakeup pin */
LL_PWR_EnableWakeUpPin(LL_PWR_WAKEUP_PIN4);
/* As default User push-button (SW1) state is high level, need to clear all wake up Flag again */
LL_PWR_ClearFlag_WU();
/* Enter the Standby mode */
HAL_PWR_EnterSTANDBYMode();
Hope it helps
2025-01-28 7:31 AM - edited 2025-01-28 7:32 AM
Hi,
Here is a code that worked for me (tested on an stm32wb15cc), based on the PWR_STANDBY_RTC example :
if( (LL_PWR_IsActiveFlag_C1SB() == 0)
|| (LL_PWR_IsActiveFlag_C2SB() == 0)
)
{
/* Set the lowest low-power mode for CPU2: shutdown mode */
LL_C2_PWR_SetPowerMode(LL_PWR_MODE_SHUTDOWN);
}
/* Enable pull down on wakeup pin PA2 */
LL_PWR_EnableGPIOPullDown(LL_PWR_GPIO_A, LL_PWR_GPIO_BIT_2);
/* Enable pull-up and pull-down configuration for CPU1 */
LL_PWR_EnablePUPDCfg();
/* Set wakeup pin polarity */
LL_PWR_SetWakeUpPinPolarityHigh(LL_PWR_WAKEUP_PIN4);
/* Enable wakeup pin */
LL_PWR_EnableWakeUpPin(LL_PWR_WAKEUP_PIN4);
/* As default User push-button (SW1) state is high level, need to clear all wake up Flag again */
LL_PWR_ClearFlag_WU();
/* Enter the Standby mode */
HAL_PWR_EnterSTANDBYMode();
Hope it helps
2025-01-28 10:54 AM
It works! I am so happy now... thank you so much!!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.