2025-02-27 4:58 AM - edited 2025-02-27 4:58 AM
Hi,
not really an issue here, but I want to understand what goes on in my BLE project.
I'm using the B-WB1M-WPAN board, starting out from the BLE_HR_p2pSensor example.
I see that my device stops advertising after I connect to it, but I can't find in the code where that happens.
I discovered that the functions:
Are used to start and stop advertising.
I also noticed that Adv_Cancel is registered as callback for a task here:
UTIL_SEQ_RegTask(1<<CFG_TASK_ADV_CANCEL_ID, UTIL_SEQ_RFU, Adv_Cancel);
Solved! Go to Solution.
2025-03-25 6:56 AM
Hello @cvlt
After putting the device in generale discoverable mode using the ACI_GAP_SET_DISCOVERABLE command, the device shall remain in general discoverable mode until a connection is established or the Host terminates the mode (using ACI_GAP_SET_NON_DISCOVERABLE command). So, the advertisement will stop after establishing a connection. More details on the Bluetooth spec V6.0[Vol 3, Part C, 9.2.4].
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-03-25 6:56 AM
Hello @cvlt
After putting the device in generale discoverable mode using the ACI_GAP_SET_DISCOVERABLE command, the device shall remain in general discoverable mode until a connection is established or the Host terminates the mode (using ACI_GAP_SET_NON_DISCOVERABLE command). So, the advertisement will stop after establishing a connection. More details on the Bluetooth spec V6.0[Vol 3, Part C, 9.2.4].
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.