cancel
Showing results for 
Search instead for 
Did you mean: 

Persisting data in BKPSRAM with STM32WBA

maborbaa
Associate II

Edited by a ST moderator to follow the community rules especially for code sharing. So please use </> to share your code

 

Hello,

I am using the STM32WBA, and I am interested in persisting data to start after waking up from standby mode.
I am unable to keep the data in memory. Here is how I am configuring the linker script and main.c.
Can you please help me with how to keep the data when waking up? I am configuring a pot for wakeup GPIO_PIN_13.
My goal is for the MCU to wake up, perform some actions, and go back to sleep repeatedly.

STM32WBA55CGUX_FLASH.ld

MEMORY
{
  RAM (xrw)   : ORIGIN = 0x20000000, LENGTH = 128K
  FLASH (rx)    : ORIGIN = 0x8000000,  LENGTH = 1024K
  BKPSRAM (xrw) : ORIGIN = 0x40024000, LENGTH = 2K
}

## after .bss:  ##

.bss_bkpsram (NOLOAD) :
{
   . = ALIGN(4);
   KEEP(*(.bss_bkpsram)) 
   . = ALIGN(4);
} > BKPSRAM

main.c

typedef struct
{
  uint32_t magic_number;
  uint16_t device_id;
} PersistentState_t;


__attribute__((section(".bss_bkpsram")))   volatile PersistentState_t g_persistent_state;

 __HAL_RCC_PWR_CLK_ENABLE();
 HAL_PWR_EnableBkUpAccess ();

if (__HAL_PWR_GET_FLAG(PWR_FLAG_SBF) != RESET)
{
        g_persistent_state.device_id++;
}
else
{
        g_persistent_state.magic_number = 0xCAFEFEED;
        g_persistent_state.device_id = 0x0001;
}

__HAL_PWR_CLEAR_FLAG(PWR_WAKEUP_FLAG2); 
HAL_PWREx_EnableStandbyIORetention (PWR_GPIO_C, GPIO_PIN_13);
HAL_PWR_EnableWakeUpPin (PWR_WAKEUP_PIN2_HIGH_1);
HAL_PWR_EnterSTANDBYMode ();

Best regards

11 REPLIES 11

I understand.

 

I understand. Thank you for all your help

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.