2017-04-25 4:11 AM
Hi,
I bought two STM32 Nucleo-L073RZ pack boards with expansion LoRa boards. I downloaded from STM32 site the example projects for board and I tried to run project for LoRa called PingPong. This project should start the communication between two boards. I unsuccessfully tried the PingPong project under IAR and also under Keil. It did not work, maybe problem in synchronization. At the beginning it works, but it fails after a some time.
I would like to ask anybody of simple source code STM32 with LoRa to run communication between two boards, simply receiver and transceiver.
Thank you,
Jan Muller#lora2017-04-25 8:52 AM
Responded earlier to PM
2017-04-26 4:36 AM
Hello Clive,
Would you mind make your response public?
May be a specific use-case/configuration leads to a particular issue with our example, it will be helpful for us and other Community members to know about it.
Thanks for your understanding.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2017-04-26 10:03 AM
No, I think that creates more busy-work for me, the PM arrived first, and I've handled it off-board. If I get feedback that my suggested changes work outside my test bench, I'll perhaps share an example.
The Ping-Pong example has meta-stability issues, it starts, it stops, it doesn't restart, the nodes get confused about what role they are playing, or can't decide. The example is also a bit superficial, if you extend or alter it to some more practical/real-world use case, you run into a number of flaws that should have been apparent when it was coded. There are issues with interrupt priorities, code in interrupt handlers blocking, and with the radio / uarts interacting badly causing data loss on both interfaces.
More generally there seems to be some issues with using the FSK build, splitting/spanning of large packets, call-backs. Now some of this may be due to a lack of appreciation about how the API is supposed to function, on my part, but the PingPong example does a poor job of illustrating how things should work, or act as a rigorous test of the API.
What is the value of doing Radio.Sleep(), and the purpose of inserting DelayMs(1) with no explanation? Why doing RadioTx() in the 'case TX:' seems to not succeed a lot of the time? Should I be able to manage data transfers in the call-backs? Are there situations where no call-backs will occur?
Not sure this is something I can hash out on the forum. Perhaps you have someone with some in-depth understanding of the API and radio stack?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.