2018-10-16 3:18 AM
Hey!
I would like to have a constant spreading factor and bandwidth when my node is transmitting data and I cannot find where I can set these parameters.
I thought I would set datarate in RegionEU868.h and control these parameters this way but it doesn't work.
Help would be much appreciated!
2018-10-16 3:32 AM
Which example specifically? Most have it as a #define up front
2018-10-18 12:12 AM
Sorry, I am talking about B-L072Z-LRWAN1 example.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.