cancel
Showing results for 
Search instead for 
Did you mean: 

Need help porting LoRa End node from L476Nuleo to L412

montezoma
Associate

So I am trying to port the cube LRWAN example for the Semtech expansion shield SX1261 from the existing Nucleo L476 to a L412 variant. I do know that it should be possible because they are not very different (Probably it is easy to do but I am simply not experienced enough).

What I did is the following :

Changing the Defines to L412XX

Changing the pin map

Generating a SystemClock_Config using CubeMX -> Copy paste into the Project

SPI is SPI2 instead of SPI1 so I changed that

Something I did not understand: What is what is the trace file used for? I guess it's just used to plot to the console so I disabled the UART (Is this a problem? )

Sadly it's not working at all (No Signal on SPI Pins...). And I am completely out of ideas.

So I need Help from a experienced ST User. If anyone has an Idea please let me know.

Thanks in advance

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.