2025-05-18 5:56 AM
I have tried to run the "UX Device HID Standalone" example under nucleo-wba65ri, and it doesn't seem to work.
I connected the board's via the USB connector to my PC and while it is recognized, in function USBX_DEVICE_HID_MOUSE_Task on line 160 both:
1. hid_mouse == UX_NULL
2. device->ux_slave_device_state == UX_DEVICE_ATTACHED and not UX_DEVICE_CONFIGURED as needed
would appreciate your support, might be imply a setup issue (I simply used a new nucleo boar and compiled and flashed the example)
Solved! Go to Solution.
2025-05-19 10:23 AM
Hello @Shaben and welcome to the ST Community.
I've test it using the STM32CubeWBA V1.6.1, the STM32CubeMX V6.14.1 and the STM32CubeIDE V1.18.1 and it works fine on my side. Could you please try it using the same material.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-05-19 10:23 AM
Hello @Shaben and welcome to the ST Community.
I've test it using the STM32CubeWBA V1.6.1, the STM32CubeMX V6.14.1 and the STM32CubeIDE V1.18.1 and it works fine on my side. Could you please try it using the same material.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.