2021-08-19 9:13 AM
Hi,
I am currently using STM32 custom board with STM32CubeWB. I am a newbee in writing the firmware. There were two versions of binary files I got from previous programmer, one is with OTA function and one is without OTA function. They were uploaded into different addresses (0x08000000 and 0x08007000).
Right now, I want to make some modifications on the firmware, and then want to generate two versions of firmware as well. But I don't know what I need to do to generate OTA and NON_OTA versions.
This is the header file I thought I can change to generate two different firmware. I thought changing the "BLE_CFG_OTA_REBOOT_CHAR" to 1 will achieve that. Apparently, it is not that easy.
Anyone could help me out?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.