2020-04-14 2:55 AM
I wanted to use the P-Nuceo-LRWAN1kit (STM32L073RZT6+SX1272) as a way to send Lora messages.
On the back the kit, thare is a message about I-CUBE-LRWAN, That uses AT commands to send Lora messages.
But wen i look voor I-CUBE-LRWAN software I canot find it working with my setup (can't find any reference of a SX1272 driver in the code as wel).
So, now I start to wonder of I-CUBE-LRWAN is only for the master side and not te slave side?
yours truly,
Jos Terra
2020-04-14 4:12 AM
There is bo such thing as a LRWAN slave. And P-Nuceo-LRWAN1kit can send and receive. However you need the right software. I think the software with the AST commands is obly available on special request (and with NDA?)You can try to adapt other software oackages.
2020-04-14 5:35 AM
One can certainly replace the firmware running inside the USI module. I used the LRWAN examples as a starting point. Not sure it is worth the effort as the Murata module has a better processor and radio. And now ST has an integrated solution.
2020-04-28 6:14 AM
Found out that the code was only to use modules like the murata module.
the Murata is, in al, wat I what I was looking for.
ps. sorry for the late response
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.