cancel
Showing results for 
Search instead for 
Did you mean: 

IPCCdataBuffAddr not matching pMb_RefTable (infinite loop)

petera88
Associate

I read the other forum on this back from 2021, but changing the files didn't do anything. Is there a fix in 2024 now?

 

 

  if (OptionsBytesStruct.IPCCdataBufAddr != (uint32_t) pMb_RefTable)
  {
    /*
     * WARNING: If there is a difference between the MAPPING_TABLE placement in memory
     * and the address calculated according to the IPCCDBA option byte,
     * to avoid writing the IPCCDBA OB by mistake, the execution enters now in a while(1){}
     * Read below, uncomment RCC_OscInitStruct local variable and replace #if 1 by #if 0 if you are sure
     */
    /* USER CODE BEGIN MBMUXIF_SystemInit_Prevent_OB_Programming */
#if 1
    /* USER CODE END MBMUXIF_SystemInit_Prevent_OB_Programming */
    Error_Handler();
#else

 

 

2 REPLIES 2
petera88
Associate

I'm actually having quite a bit of trouble starting an STM32WL55JC project, and activating SubGHz radio. The generated code doesn't work. How necessary is the MbMux framework? Is there anyway to get a minimal application going? 

None of the dual core example project seem to work.

Hello @petera88 

If you are looking for a SUBGHZ, I may suggest you take a look at the SubGHz_Phy_PingPong_DualCore example. It should help you.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.