2025-08-12 5:31 AM
When using the version v2024.08.14-nightly described in the Wiki, configuring and outputting with the ZAP tool does not include GeneralCommissioning inside DispatchSingleClusterCommand in IMClusterCommandHandler.cpp. This causes a build error.
Could you please explain the cause?
2025-08-12 6:00 AM
Hello @AkihiroN
Could you please give more details about this behavior and how to reproduce it.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-08-12 7:55 AM
Understood.
The development environment is as follows:
・X-Cube-Matter: v1.4.1
・zap tool: v2024.08.14-nightly
・STM32CubeIDE: v1.17
Base project: Lighting-App-SBSFU
・Reproduction steps:
Step 1: Use the zap tool to create a .zap file (attached)
Step 2: Use generate.py and codegen.py to generate the necessary files
Step 3: Rename the Lighting-App-SBSFU project and open it in STM32CubeIDE
Step 4: Link the generated files accordingly
Step 5: Build the project. The build succeeds.
Step 6: Execute commissioning. When executing, commissioning fails because there is no case statement for case Clusters::GeneralCommissioning::Id: in IMClusterCommandHandler.cpp (GeneralCommissioning server is enabled in the ZAP tool)
Why is the DispatchSingleClusterCommand for GeneralCommissioning not generated even though GeneralCommissioning is enabled in the ZAP tool?
In the Lighting-App-SBSFU project inside X-Cube-Matter v1.4.1, the IMClusterCommandHandler.cpp within the lighting-app does have GeneralCommissioning enabled. However, using lighting-app.zap and generating files with zap tool v2024.08.14-nightly results in the same issue.
Could you please tell me the version of the zap tool used for the Lighting-App-SBSFU?
2025-08-13 6:52 AM
Hello @AkihiroN
Could you please try using the X-Cube-Matter V1.4.2, the STM32CubeIDE V1.19.0, the STM32CubeWB V1.23.0 and the ZAP tool version v2025.07.24.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-08-13 7:23 PM
2025-08-13 7:41 PM
Sorry for the repeated requests.
Could you please generate the related files using the .zap file I shared earlier?
Also, I would like you to check whether the case statement for case Clusters::GeneralCommissioning::Id: is generated inside IMClusterCommandHandler.cpp.
2025-08-31 7:41 PM
How is the situation progressing?
Could you please let me know the version of the ZAP tool used in 1.4.2?
Also, could you send me the IMClusterCommandHandler.cpp file generated based on the test.txt (ZAP file) I attached the other day using that version?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.