2021-08-02 5:33 AM
Hi,
I'm taking an STM32wb55 based PCB through CE testing. The test house require the following information which I haven't got.
Modulation scheme
Duty cycles
Channel hopping
Worst case operational modes
Transmit operational modes
Medium Utilization
Any information would be helpful.
Rhydian
2021-08-12 5:51 AM
What type of info regarding Duty Cycle are you looking for?
>Worst case operational modes
Dp you mean in a noisy environment with blockers inside and outside the BLE band?
2021-08-13 12:36 AM
For the CE certification for BLE devices, you must be compliant with EN 300 328 V2.2.2 :
Modulation scheme GFSK modulation width 2MHz
Duty cycles -> 98%
Channel hopping No -> DSSS
Worst case operational modes 2MHz
Transmit operational modes Permanent with modulation
Medium Utilization No
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.