2021-08-18 5:02 PM
I have written an app using the sequencer and time server. My app selectively runs or doesn't run the BLE stack by calling or not appe_Tl_Init();
I use HW_TS to generate delays. When I don't run the appe_Tl_Init function my timing is correct. when I do run the function the timing is 4 times too fast. How does appe_Tl_Init() affect this timing?
Solved! Go to Solution.
2021-08-19 8:35 AM
appe_Tl_Init should not affect the timers. This function is initializing the IPCC system before releasing the CPU2 for booting.
Now CPU2 is indeed setting its own parameters/dividers for the RTC. The RTC is the time base for the timers used to pace the BLE communication accurately.
So some settings may disturb your time base when CPU2 is activated.
You could try with another application like the p2pServer project to check whether you face the same issue.
2021-08-19 8:35 AM
appe_Tl_Init should not affect the timers. This function is initializing the IPCC system before releasing the CPU2 for booting.
Now CPU2 is indeed setting its own parameters/dividers for the RTC. The RTC is the time base for the timers used to pace the BLE communication accurately.
So some settings may disturb your time base when CPU2 is activated.
You could try with another application like the p2pServer project to check whether you face the same issue.
2021-08-19 12:55 PM
Thanks. I have fixed (hopefully) the problem. I had several timers defined, but only Created some of them. The I removed the unused timers the problem went away.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.