2025-08-19 8:21 AM
Hey,
I am trying to make a device which connect to an app using stm32wb15. Everything works properly, but I want to make it so that when the device becomes disconnected, i can use a button to broadcast BLE so that i can connect through an app again. I tried the existing ready functions. But I could not seem to make it visible as a Bluetooth device again (have to restart the device)
Can someone point me to which functions i should call in the main.c to start broadcasting durign button press.
Solved! Go to Solution.
2025-08-20 4:18 AM
Hello,
for advertising you can use Adv_Request(APP_BLE_FAST_ADV) function.
CFG_TASK_ADV_CANCEL_ID is ID for the task that cancels the advertising.
You need this ID for registering and running the task in the sequencer (scheduler for tasks).
Please read this document below as it might be helpful for you.
How to build wireless applications with STM32WB MCUs - Application note
I recommend reading section 4.4/4.5 and 7.
If you have any question, please don't hesitate to ask.
You could also share the project if it is possible, so I could help you further with your application.
Best regards,
Filip Kremen
2025-08-19 11:24 PM
Hello,
I would suggest creating a task for start advertising (in the same way as CFG_TASK_ADV_CANCEL_ID) and then you can call Adv_Start_Req (Adv_Cancel_Req for cancel advertising) from one of the APP_BLE_Key_ButtonX_Action function. Please let me know if it works on your side.
Best regards,
Filip Kremen
2025-08-20 2:08 AM
Hi, I am new to this. So i do not understand what i should do. CFG_TASK_ADV_CANCEL_ID ?
Here is what i have:
static void Button_Check(void)
{
uint8_t button_current_state = HAL_GPIO_ReadPin(button_GPIO_Port, button_Pin);
uint32_t current_time = HAL_GetTick();
if (button_last_state == 0 && button_current_state == 1) {
if (current_time - last_button_time > 100) {
last_button_time = current_time;
// 1. Confirmation vibration
Vibration_Pulse(100);
// 2. Direct BLE stack call (no external dependencies)
aci_gap_set_non_discoverable();
HAL_Delay(500);
// Start advertising with direct call
tBleStatus ret = aci_gap_set_discoverable(
ADV_IND, // Advertising type
0x0020, // Min interval (20ms)
0x0040, // Max interval (40ms)
0x00, // Own address type
NO_WHITE_LIST_USE, // No whitelist
7, // Local name length
(uint8_t*)"BackTra", // Device name
0, // Service UUID length
NULL, // Service UUIDs
0x0006, // Min conn interval
0x0C80 // Max conn interval
);
// 3. Feedback based on result
if (ret == BLE_STATUS_SUCCESS) {
// Success: 3 quick vibrations
Vibration_Pulse(100);
HAL_Delay(100);
Vibration_Pulse(100);
HAL_Delay(100);
Vibration_Pulse(100);
} else {
// Failed: 1 long vibration
Vibration_Pulse(500);
}
}
}
button_last_state = button_current_state;
}
I saw this as well, and i tried using it, but it did not work. Can you tell me which function from the app_ble i should call to start advertising?
/**
* Start to Advertise to be connected by P2P Client
*/
Adv_Request(APP_BLE_FAST_ADV);
/* USER CODE BEGIN APP_BLE_Init_2 */
/* USER CODE END APP_BLE_Init_2 */
2025-08-20 4:18 AM
Hello,
for advertising you can use Adv_Request(APP_BLE_FAST_ADV) function.
CFG_TASK_ADV_CANCEL_ID is ID for the task that cancels the advertising.
You need this ID for registering and running the task in the sequencer (scheduler for tasks).
Please read this document below as it might be helpful for you.
How to build wireless applications with STM32WB MCUs - Application note
I recommend reading section 4.4/4.5 and 7.
If you have any question, please don't hesitate to ask.
You could also share the project if it is possible, so I could help you further with your application.
Best regards,
Filip Kremen
2025-08-20 9:12 AM - edited 2025-08-20 9:13 AM
Hey. I read about sequencing and Now it works! Thank you.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.