2020-02-06 11:07 PM
Hello everyone,
I am working on B L072Z LRWAN1 kit, in which murata LoRa Module is used having STM32L072 controller.
I am trying to implement low power modes and running the example code :
STM32Cube\Repository\STM32Cube_FW_L0_V1.11.2\Projects\STM32L073Z-EVAL\Examples\PWR\PWR_STOP_RTC
I am directly running this code on my board, but it is not working. While debugging i found that it is in infinite loop during clock configuration.
Please guide me regarding this and settings i need to do.
Thanks
Shubham
2020-02-07 1:50 AM
If it goes into the Error_Handler or a while(1) loop it is likely one or more of the clock parameters doesn't match the settings of the board. For example the HSE_VALUE
Compare and contrast the settings vs those of working LRWAN examples.
2020-02-07 2:15 AM
I didn't change anything, i just run the example given by STM for this board.
There is nothing i can found about this module, no example code, no documents.
If you have something reference document of the apis and settings where i can look and would be able to do the settings my own, please share.
Regards
Shubham
2020-02-10 4:08 AM
Hi,
I cross checked the settings and did the same settings as per thr LRWAN1 ping pong example, but still the same issue.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.