2020-06-18 9:12 AM
I have made my own board using the STM32WB55CGU processor (the 48 pin package, as used on the Nucleo Dongle, MB1293C.
I am now trying to get the BLE working and tuned. The first step, it seems, is to load the transparent mode firmware into the chip which passes the USART TX & RX through to the BLE stack. It seems the firmware in the title should do this, but it is currently using the VCP, and I don't have the USB broken out on my board, so I can't use this. I do, however, have the USART coming out.
Is there a simple way of switching this over to the USART in the sample code? I am using the STM32CubeIDE, and have imported the project, but it does not include the CubeMX file.
2020-06-19 2:08 AM
I ended up rolling my own solution by calling hci_send_req(..)
#define OGF(hci_packet) (hci_packet[1] >> 2)
#define OCF(hci_packet) (hci_packet[0] | ((hci_packet[1] & 0x03) << 8))
extern UART_HandleTypeDef huart1;
tBleStatus genericHciCommand(uint8_t *hci_packet, uint8_t packet_length,
uint8_t *ret_buffer, uint8_t *ret_buffer_len) {
struct hci_request rq;
tBleStatus *status = &ret_buffer[0];
Osal_MemSet(&rq, 0, sizeof(rq));
rq.ogf = OGF(hci_packet);
rq.ocf = OCF(hci_packet);
rq.cparam = &hci_packet[3];
rq.clen = packet_length - 3; // 3 = 2 bytes opcode (ogf + ocf) and param 1 byte length
rq.rparam = ret_buffer;
rq.rlen = *ret_buffer_len;
if (hci_send_req(&rq, FALSE) < 0)
return BLE_STATUS_TIMEOUT;
if (*status) {
*ret_buffer_len = rq.rlen;
return *status;
}
*ret_buffer_len = rq.rlen;
return BLE_STATUS_SUCCESS;
}
#define HCI_PARAM_LEN(hci_packet) (hci_packet[2])
void testBle() {
hci_reset();
uint8_t ret_buffer[BLE_EVT_MAX_PARAM_LEN];
uint8_t cmd_buffer[BLE_CMD_MAX_PARAM_LEN + 3];
while (1) {
HAL_StatusTypeDef error = HAL_OK;
uint8_t hci_cmd_header = 0;
error = HAL_UART_Receive(&huart1, &hci_cmd_header, 1, 1000);
if (error != HAL_OK || hci_cmd_header != 0x01) {
continue;
}
memset(cmd_buffer, 0, BLE_CMD_MAX_PARAM_LEN + 3);
error = HAL_UART_Receive(&huart1, cmd_buffer, 3, 1000);
if (error != HAL_OK) {
continue;
}
if (HCI_PARAM_LEN(cmd_buffer)) {
error = HAL_UART_Receive(&huart1, &cmd_buffer[3], cmd_buffer[2],
1000);
if (error != HAL_OK) {
continue;
}
}
uint8_t ret_param_len = BLE_EVT_MAX_PARAM_LEN;
genericHciCommand(cmd_buffer, cmd_buffer[3], ret_buffer,
&ret_param_len);
// hci_send_req removes the event code, num commands and opcode and only delivers parameters in ret_buffer
uint8_t cmd_cplt_resp_header[6] = { 0x04, 0x0E, ret_param_len + 3, 1,
cmd_buffer[0], cmd_buffer[1] };
HAL_UART_Transmit(&huart1, cmd_cplt_resp_header, 6, UINT32_MAX);
HAL_UART_Transmit(&huart1, ret_buffer, ret_param_len, UINT32_MAX);
}
}This function runs in an endless loop. If you implement that differently you might want to make sure you don't call UTIL_SEQ_Run() to make sure this procedure is not disturbed by other actions.
2020-06-28 1:35 AM
@HRadt.1 Thank you for that. I need to go through your code a bit at a time as it is beyond me at the moment! In the end, I took the transparent mode code from the actual nucleo board and copy and pasted all the differences from a basic project for the different chip, which (surprisingly) worked!
Thanks again for your help!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.