2025-01-29 2:33 AM - last edited on 2025-01-30 12:54 AM by ELABI.1
I am looking to know where I should write HCI commands. For example I need to write HCI_LE_SET_PHY . Should I use STM32CubeMonitor-RF. If yes, then I don't find BLE_TransparentMode for STM32WB35XX series.
please let know
2025-01-29 5:31 AM
Hi @Nico3
You can refer to this application note AN5270. It provides a list of supported commands, and you can specifically see section 2.1.57, HCI_LE_SET_PHY, which discusses the HCI_LE_SET_PHY command.
Thank you.
ELABI.1
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-01-29 6:00 AM
Thanks, I looked at AN5270.. But my question is where i should put the command in my Application code. As these are low level commands, I am afraid for damaging the BLE. Any code example ??
2025-01-30 1:07 AM - edited 2025-03-05 5:45 AM
Hi @Nico3,
For the STM32WB35, we don't have any specific application.
I suggest you have a look at one of our examples on the STM32WB55 and debug it to understand how your command is exactly implemented. After that, you can migrate the implementation from the STM32WB55 to the STM32WB35 using the AN451.
There isn't any specific place to write your command, it depends on your project.
Thank you.
ELABI.1
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.